S12ZVL LIN TxD dominant timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVL LIN TxD dominant timeout

1,582件の閲覧回数
Abor88
Contributor I

Hello,

in my application I am using S12ZVL128 and LIN. I am using CodeWarrior and ProcessorExpert in my project.

LINPHY is routed to SCI0 and all is working properly.

Now I would like to detect if LIN bus is shorted to GND and (I think) it could be reach implementing the detection of TxD-dominant timeout feature (please, correct me if I am wrong).

In Processor Expert I enable TxD-dominant feature and I have verified that LPDTIE = 1 after the code generation, as expected. I have also configured the ISR callback but ISR is never reached.

Are there some other configurations to be done in order to enable this feature?

Thanks and regards,

Andrea

0 件の賞賛
返信
1 返信

1,562件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

 

Hi,

 

You wrote you set LPDTIE but..

 

LPDTIE, LIN transmitter TxD-dominant timeout Interrupt Enable

0 Interrupt request is disabled.  /   1 Interrupt is requested if LPDTIF bit is set.

 

LPOCIE - LIN transmitter Overcurrent Interrupt Enable

0 Interrupt request is disabled.  /   1 Interrupt is requested if LPOCIF bit is set.

 

 

Also check you have enabled global interrupt enable….. from the CPU manual

 

7.3.5 I-bit-Maskable Interrupt Requests

Maskable interrupt sources include on-chip peripheral systems and external interrupt service requests. Interrupts from these sources are recognized when the global interrupt mask bit (I) in the CCR is cleared. The default state of the I-bit out of reset is 1, but it can be written at any time if the CPU is not in user state. The interrupt module manages maskable interrupt priorities. Typically, an on-chip interrupt source is subject to masking by associated bits in control registers in addition to global masking by the I-bit in the CCR. Sources generally must be enabled by writing one or more bits in associated control registers. There may be other interrupt-related control bits and flags, and there may be specific register read-write sequences associated with interrupt service. Refer to individual on-chip peripheral descriptions for details.

 

BTW, we do not suggest to use PE as development  platform because the evolution was closed long time ago and no bug will be neither investigated nor corrected. Of course, it is suitable to be used as teaching tool, but from my experience, it is better to have everything under own control.

 

Best regards,

Ladislav

0 件の賞賛
返信