Regarding IDE to be used for MC9S12DT256CPVE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding IDE to be used for MC9S12DT256CPVE?

1,128 Views
sourabhjain
Contributor III

Hi,

 

i am using MC9S12DT256CPVE processor HCS12 core. 

Which IDE  and version should i used?

0 Kudos
7 Replies

869 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

It depends on which operating system do you use.

So, if you are using one of the host platforms below I would like to recommend you the CodeWarrior version 5.1

• Host Platforms:

Windows® XP 32-bit and 64-bit (Professional Edition)

Windows Vista 32-bit and 64-bit (Business)

Windows Vista 32-bit (Home Premium)

Windows 7 32-bit and 64-bit (Professional Edition)

Windows 7 32-bit and 64-bit (Home Premium) 

For the download, please, open the link below and click on the Download Eval button. After that, select the Previous tab. There can be found the installation link.

 CodeWarrior® Dev Tools for HCS12(X) MCUs | NXP 

If you are using bellow platforms you need to use the CodeWarrior version 5.2.

Microsoft Windows 8 32- and 64-bit

Microsoft Windows 8.1 32- and 64-bit

Microsoft Windows 10 32- and 64-bit

But this version does not include the S12D Family so, you need to add this MCU to the CodeWarrior 5.2 by this procedure: How-to Add missing derivatives to CodeWarrior Classic HCS12(X) 5.2 (Unofficial Method) 

The download link is the same. Just select the Current tab instead of the Previous tab.

I hope it helps you. If you have any questions, let me know.

Best Regards,

Diana

0 Kudos

869 Views
sourabhjain
Contributor III

pastedImage_1.png

Hi,

Which IDE categories should i used in attached snapshot ?

0 Kudos

869 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi, 

The CodeWarrior Evaluation license (based on the Professional Suite) is time-limited usually 30 - 45 days.

After that, it is a Special Edition (Free Tool).

The restriction only lies in the software feature. So, it is up to you if the special edition fill your requirements or you buy the CW license (Basic/Standard/Professional)

Also, you can look at the details on the link below:

https://www.nxp.com/docs/en/fact-sheet/950-00437.pdf 

I hope it helps.

Best Regards,

Diana

0 Kudos

869 Views
sourabhjain
Contributor III

Hi Diana,

Thank you for the inputs.

I want to know that this Code Warrior supports universal multilink FX debugger?

0 Kudos

869 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, the Multilink FX is supported by CodeWarrior 10.2 and higher:

PEmicro | Experts in Embedded tools for Flash Programming and Development 

You can use, for example, USB Multilink Universal instead which is supported by CodeWarrior v 5.1/5.2

MULTILINK | Debug Probe | PEmicro 

Best Regards,

Diana

0 Kudos

869 Views
sourabhjain
Contributor III

Hi Diana,

Should i used LauterBach Trace 32 IDE for MC9S12DT256CPVE processor HCS12 core?

Is USB multilink universal debugger is supported for Trace 32?

Regards,

Sourabh

0 Kudos

869 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

It is up to you which debugger and tools you want to use.

Trace 32 is an advanced tool. I'm afraid that USB Multilink Universal debugger is not supported by Trace 32. 

Best Regards,

Diana

0 Kudos