I have a program with the following two sets of data:
// a list of ADDRESSES of BYTEs #pragma INTO_ROM const byte * These_Data[]={ &P12.b.high, &P12.b.low, &N12.b.high, &N12.b.low, &HVDC.b.high, &HVDC.b.low, ...... }; #pragma INTO_ROM // a list of LITERAL BYTEs const byte These_Codes[] ={ P12_HB, P12_LB, N12_HB, N12_LB, HVDC_HB, HVDC_LB, ...... };
The first is a list of addresses of data in SRAM... some words, some bytes, some longs, but all addressed as bytes
The second is a list of literal byte-values that will be sent along with the data found at the associated addresses.
No matter what I do, the LITERALS are compiled into ROM and the ADDRESSES end up in SRAM.
I'm not (yet) hurting for space, but it bugs me that data that is obviously (to me) invariant is always put in R/W memory.
What am I missing?
(9S12DX256, CW 5.90)
Thanks for any illumination
Wade Hassler
Dear Wade,
Try adding a second const . All you've done so far is say that the things pointed AT are constant - not the array itself.
#pragma INTO_ROM const byte * const These_Data[]={&P12.b.high, &P12.b.low,&N12.b.high, &N12.b.low, &HVDC.b.high, &HVDC.b.low,...... };
You didn't say what target but a similar example worked on CFV1 (Eclipse)
bye