PROG12Z is throwing invalid addresses in srecord block

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PROG12Z is throwing invalid addresses in srecord block

跳至解决方案
1,015 次查看
ganeshvijayakum
Contributor I

Hi,

 

I am trying to flash .phy file of my Bootloader software using Cyclone pro through PROG12Z tool.

 

when I flash my code through CodeWarrior IDE debug mode my code runs without any problem.

But when I try to flash .phy file the PROG12Z tool is throwing the following error,

160006_160006.pngpastedImage_1.png

 

For your information I am using the burner file attached, to compile using the IDE CodeWarrior.

 

Well I use the algorithms to erase and link are as mentioned below,

Freescale_9S12G128_1x16x2k_4k_EEPROM.12P

Freescale_9S12G128_1x16x64k_128k_Linear_Pflash.12P

 

Please let me know why am I getting Invalid address in srecord block?

 

Is it related to burner file? If yes, I request you to provide me the burner file needed for S12G micro.

 

Thanks & Regards,

Ganesh Vijaya Kumar P.

Original Attachment has been moved to: burner.bbl.zip

标签 (1)
0 项奖励
回复
1 解答
653 次查看
iggi
NXP Employee
NXP Employee

Hi Ganesh,

Please try and convert the .phy file you use with PEMicro's Log2phy tool:

PEMicro Blog


or SRecCvt tool:

SRECCVTSW (REV 1.0.31)

p.s. The burner file for S12G devices generated by CW was not correct as it was taken from older MCUs. That was reported and fixed. The one you attached differs from a random one i took from a CW project (see attached0).

Regards,

iggi

在原帖中查看解决方案

0 项奖励
回复
2 回复数
654 次查看
iggi
NXP Employee
NXP Employee

Hi Ganesh,

Please try and convert the .phy file you use with PEMicro's Log2phy tool:

PEMicro Blog


or SRecCvt tool:

SRECCVTSW (REV 1.0.31)

p.s. The burner file for S12G devices generated by CW was not correct as it was taken from older MCUs. That was reported and fixed. The one you attached differs from a random one i took from a CW project (see attached0).

Regards,

iggi

0 项奖励
回复
653 次查看
ganeshvijayakum
Contributor I

Hello Iggi,

The burner.bbl file you have attached above has resolved the problem.

I appreciate your  support.

Thank you & Regards,

Ganesh Vijaya Kumar P.

0 项奖励
回复