Need your help with MC9S12DT256B (printing integers or characters in sequence on the LCD display)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need your help with MC9S12DT256B (printing integers or characters in sequence on the LCD display)

951件の閲覧回数
Aditya
Contributor I

Hello, I was looking a demo application for MC9S12DT256B which prints characters & strings onto the LCD display using LCDPutString() and LCDPutChar() function.

 

(a)  My requirement is to print integers in a loop (say i = 0 to i = 10) onto the LCD display. Can you kindly help me out with this? I tried a number of ways to implement it, but unfornately none of them worked.

 

(b) As I can print characters using LCDPutChar function, is it possible to print the characters on the LCD display in sequence by incrementing the ascii values? Please help me out with this.

 

Thanks,

Aditya.

ラベル(1)
0 件の賞賛
1 返信

307件の閲覧回数
RaviKashi
Contributor I

If you already have a function that is able to print the chars (LCDPutChar) then all you have to do is

 

for ( i = 0; i  < 10; i++ ){   LCDPutChar( 0x30 + i );      Delay ( 2ms ); /* Delay of 2 ms if you are not watching the busy flag */}

It be an idea to post the things that you have tried so that we dont suggest what you have already tried or see if there is a bug in what you have done. The above will print 0 to 9 like

 

0123456789,  depending on if this the first thing that your are printing after clearing the LCD and commanding it to home position.

 

Message Edited by Ravi Kashi on 2009-04-19 11:12 AM
0 件の賞賛