MC9S12XET256 - AD conversion only returns values with gaps of 64, 32 or 16.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12XET256 - AD conversion only returns values with gaps of 64, 32 or 16.

Jump to solution
947 Views
LeandroLeite
Contributor II

Hello,

 

I'm working with analogic to digital conversion in the MC9S12XET256, but the ATD module is returning strange values. If the signal voltage is less than 2.5V the ATD returns 0, and when the signal is higher than 4.0V it returns 1023 (in 10Bits resolution mode).

 

But the most curious happens when the signal is between 2.5V and 4.0V. The AD conversion becomes very instable and returns only values with gaps of 64, 32 or 16, depending of voltage level. Below are the values that I got: In the left column are the results that I got from AD conversion (resolution of 10Bits), and in the right column the differences between the left value and the one just below. The conversion never returns values between the ones specified below, like 978, 678 or 115.

1023 63

960 64

896 64

832 64

768 64

704 64

640 64

576 64

512 64

448 64

384 64

320 64

256 32

224 32

192 32

160 32

128 16

112 16

96

 

The code is:

ATD configuration registers set as:

ATD0CTL1 = ATD0CTL1_SRES0_MASK; // Resolution of 10Bits

ATD0CTL2 = ATD0CTL2_ASCIE_MASK;  // Interrupt enabled

ATD0CTL3 =  ATD0CTL3_DJM_MASK |   // Right justified result

                         ATD0CTL3_S1C_MASK |   // S1C|S4C:  5 channels read

                         ATD0CTL3_S4C_MASK;

ATD0CTL4 =  ATD0CTL4_SMP2_MASK | // 12 ATD clock cycles sample time

                         19;// prescaler value of 19; 40MHz fBUS >> 1MHz fATDCLK


To start a conversion, I do:

ATD0CTL5 = ATD0CTL5_MULT_MASK;


When the conversion is done a Xgate interrupt is generated, and inside the Xgate code I read the values of ATD0DR. The problem isn't caused by interrupts, once that codes without interrupts shows the same strange values. It seems that the ATD clock frequency is too high, but the problem persists even when the ATD Clock is only 1MHz.

 

Can it be a physical (device) problem? Maybe the "conversion complete flag" is being set too early, I don't know. Please help!

 

Thanks in advance,

Leandro

Labels (1)
0 Kudos
Reply
1 Solution
700 Views
kef
Specialist I

What about VDDA, VSSA, VRH, VRL pins connections? Are these properly decoupled? What is source impedance, isn't it to high?

View solution in original post

0 Kudos
Reply
2 Replies
701 Views
kef
Specialist I

What about VDDA, VSSA, VRH, VRL pins connections? Are these properly decoupled? What is source impedance, isn't it to high?

0 Kudos
Reply
700 Views
LeandroLeite
Contributor II

Hi Kef,

 

The source impedance and decoupling were correct, we followed the instructions of datasheets and applications notes.

 

But when I saw your answer I decided to double check the pins VDDA, VSSA, VRH and VRL. VDDA and VSSA were ok, but pins VRH and VRL weren't well soldered to the board - the pads (contact) below the pins were in the correct voltage but the pins were floating. So I re-soldered it, adding a little more solder, and the ATD works perfectly!

 

Thank you for helping me find the solution!

Leandro

0 Kudos
Reply