MC9S12DP256B problem on a M68EVB912DP256 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S12DP256B problem on a M68EVB912DP256 board

2,238 次查看
Ashwin
Contributor I
Hello,
I am using a MC9S12DP256B chip (1K79X;HZDH0203) on a M68EVB912DP256 evaluation board. I have a BDM-Multilink cable. I have the following problem:
 
According to the ICD-12 manual, I am not able to see the same list of stationeries(when the HC12 stationery is chosen in the new project). This is what I am seeing:
Board Support:
9s12badge
cml12s-dp256
evb912dp256
HCS12 T-board
HCS12_Stationery
_A128_L40K
_A256_L91N
_A512_L00M
_A64_L86D
_C32_L45J
_DP256_K79X
_Dx256_L91N
_Dx512_L00M
_Dx64_L86D
_E128_L15P
_E64_L15P
_H128_K78X
_H256_K78X
_MC9212_ALL
 
I tried the EVB912DP256, MC9S_all, _DP256_K79X,912Sbadge, HC12 T-board. Each time, I tried to make and debug the project, I get the same error that the board could not be found. It is unable to connect to the board. What should I do?
标签 (1)
0 项奖励
1 回复

428 次查看
Alban
Senior Contributor II
Hi Ashwin,
 
For you to get something working very quickly, instead of selecting the "Stationary", use the project wizard for the "P&E Micro ICD" target.
This will create all the files and startup code necessary for your project to work.
 
From there, you can see how things are working together to create a project yourself if you wish to do so.
 
Good Luck :smileytongue:
Alban.
0 项奖励