I need mention of s12zvm_PMSMFOC_appcfonfig.xls 

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need mention of s12zvm_PMSMFOC_appcfonfig.xls 

1,218 Views
ahnjoseph
Contributor III

Hi

 

I tried PMSM FOC with attach file

So, I need kindly mention of Configuration S12ZVM_PMSMFOC_appcfonfig.xls

Specially, Please look below Picture

 

i did attach project file

153188_153188.pngpastedImage_0.png

 

153189_153189.pngpastedImage_1.png

153191_153191.pngpastedImage_3.png

Original Attachment has been moved to: MTRCKTSPNZVM128-SW.exe.zip

Labels (1)
0 Kudos
4 Replies

982 Views
ahnjoseph
Contributor III

Thank`s your Kindly mention .!

0 Kudos

982 Views
RadekS
NXP Employee
NXP Employee

Hi Ahn,

Could you please clarify what you mean by “mention of Configuration S12ZVM_PMSMFOC_appcfonfig.xls”?

Do you need to explain what does these calculators and constants? Or you need to check whether target values are OK?

Have a great day,
Radek

0 Kudos

982 Views
ahnjoseph
Contributor III

Hi Radeks

Thanks your interest my question

FOC Setup

Current loop sampling period

CLOOP_TS

100.0E-6

Current loop bandwidth

CFOC_F0

400

Current loop attenuation

CFOC_ATT

0.9

Q1 : What is mean “Current loop sampling period”

Q2 : What is mean “Current loop bandwidth”?

Q3 : What is mean “Current loop attenuation”?

Q4 How can I tuning upper Questions Value with Freemaster ?

Thank you kindly answer

Best Regards

……………………………………

Joseph Ahn(안연수)

Assistant Software Design Manager

Avnet Electronic Marketing.

Joseph.ahn@avnet.com<mailto:Joseph.ahn@avnet.com>

……………………………………

12th Floor, KBS Media Center, Maebongsan-ro 45 (Sangam-dong),

Mapo-gu, Seoul, 121-915, Korea

Direct:

82-2-6277-6395

Fax:

82-2-761-2133

0 Kudos

982 Views
RadekS
NXP Employee
NXP Employee

Hi Joseph,

In normal run, the motor is driven by two closed loops.

The fast loop is executed typically every 100us and we call it the Current loop.

The slow loop is executed typically every 1ms and we call it the Speed loop.

The Current loop:

The current loop.png

From Current loop bandwidth and Current loop attenuation parameters are recalculated PI regulators parameters.

The typical value for Current loop bandwidth is 200~250Hz and for Current loop attenuation it is 0.8~0.9.

For more details, please look at application note AN5135:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN5135.pdf

or look at theory by searching something like “close loop feedback control”.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------