GDU init as follwing:
void initGDU(void)
{
GDUE_GCPE = 1; // charge pump
GDUE_GCSE0 = 1; // enable Current Sense Amplifier 0
GDUF = 0xff; // Flag Register - clear all error flags
GDUBCL = 0x0F; // Set coil current limit to maximum 750mA
GDUCLK1_GBOCD = 0b10001; // Set boost frequency ~ 0.52MHz
GDUCLK1_GBODC = 0b11; // Set duty cycle to 75%
GDUE_GBOE = 1; // Enable boost
GDUCLK2_GCPCD = 2; // Fbus / 32
GDUCTR = 0x93;//0x13; // blanking time
GDUDSLVL = 0x77; // desat. level
GDUE_GFDE = 1; // enable FET pre-driver
GDUDSE = 0x77; // Clear Desaturation Error Flags
}
The Schematic like this,
I use Oscilloscope test CP pins, the output single like this
I set Frequence = 0.52MHz, but output Frequence is 0.39MHz, the duty i set is 75%, but the output is 50%.
so i want to know how to correct it.
Thank you Very much.
解決済! 解決策の投稿を見る。
Hello,
The GDUCLK1 register is not for the Charge Pump but for the Boost Converter.
The Charge Pump Output Pin (CP) switches with 50% duty cycle and its frequency is configurable in the GDUCLK2 register.
Regards,
Daniel
Hello,
The GDUCLK1 register is not for the Charge Pump but for the Boost Converter.
The Charge Pump Output Pin (CP) switches with 50% duty cycle and its frequency is configurable in the GDUCLK2 register.
Regards,
Daniel
Hi Daniel,
Thank you so much, this problem was solved according to your statement.
Brs,
Chao.Ding