Does the S9S12XS256J0MAER support BSDL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the S9S12XS256J0MAER support BSDL?

544件の閲覧回数
maximilianweiss
Contributor I

Does the S9S12XS256J0MAER Support BSDL. I need an BSDL-File for the Controller.

ラベル(1)
0 件の賞賛
1 返信

478件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Maximilian,

S12 devices do not use JTAG interface. Therefore I am afraid that we do not provide BSDL file for S12XS MCUs.

S12XS MCUs are programmed and debugged trough BDM interface.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛