Can S12ZVCA work in 3.3V ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can S12ZVCA work in 3.3V ?

Jump to solution
1,018 Views
Robin_9411
Contributor I

Hi,

I‘m using a S12ZVCA64, I want to disable internal voltage regulator(output 5V) and connect 3.3V supply to VDDX1, I have set CPMUVREGCTL = 0x06 which disable internal voltage regulator, but I measured the VDDX1 voltage is 4.3V, not 3.3V.

Anyone can help me? Thanks!!!

0 Kudos
1 Solution
963 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Robin_9411,

You would need to connect VSUP = VDDX = VDDA = VDDC to the 3.3V regulator.

This should be feasible, but it is not an official usecase, it has not been validated by NXP.

The official usecase is to use the internal regulator either with the internal or an external ballast transistor.

 

BR, Daniel

View solution in original post

0 Kudos
2 Replies
964 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Robin_9411,

You would need to connect VSUP = VDDX = VDDA = VDDC to the 3.3V regulator.

This should be feasible, but it is not an official usecase, it has not been validated by NXP.

The official usecase is to use the internal regulator either with the internal or an external ballast transistor.

 

BR, Daniel

0 Kudos
951 Views
Robin_9411
Contributor I

Hi Daniel,

Thank you very much! It worked !

BR, Robin

0 Kudos