Can AD conversion detect negative voltage?(I use S12ZVL family)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can AD conversion detect negative voltage?(I use S12ZVL family)

916件の閲覧回数
Jen1
Contributor I

微信图片_20220413142045.png

DJM: Result Register Data Justification — Conversion result data format is always unsigned. This bit controls justification of conversion result data in the conversion result list.

Q: I want to detect the negative voltage in the circuit, but according to the data manual, the conversion result is always unsigned. How can I detect the negative voltage with sign?  

0 件の賞賛
返信
3 返答(返信)

898件の閲覧回数
Jen1
Contributor I

Thank you very much for your answer.

I have some other question:  Can I measure more than 9 volts or 16v?

0 件の賞賛
返信

889件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Yes, it is, using HVI (High Voltage Inputs).

Please refer to the S12ZVL RM.

2.4.5 High-Voltage Input

J.1 High-Voltage Inputs (HVI) Electrical Characteristics.

danielmartynek_0-1649924397599.png

 

BR, Daniel

 

0 件の賞賛
返信

906件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Jen1,

The ADC can't measure negative voltage.

The input voltage (V_IN) must be within the <V_RL; V_RH> range.

danielmartynek_0-1649854192604.png

If negative voltage (V_IN < VSSA) is applied to a pin, the voltage is clamped to VSS.

Please refer to the S12ZVL RM,

C.1.1.4 Current Injection.

A.1.2 Current Injection

Table A-10. 5V I/O Characteristics (Junction Temperature From –40C To +175C)

danielmartynek_1-1649854462139.png

 

Regards,

Daniel

0 件の賞賛
返信