I want to implement 6 independent output PWM on S9ZVML128.
或者我该怎么配置寄存器,我现在一头雾水
我想要6路独立的pwm输出到GDU上,有相应的程序吗?
Hi,
ZVML128 provides you to use 6 independent PMF channels (enhanced motor control oriented PWM with fault protection) if you do not use GDU module and connects PMF to GPIO pins. If you use GDU module then it blocks simultaneous active top and bottom part of the H bridge leg (complementary pair). Also, you can use TIM module to generate 4 independent simple PMW.
Note, S12ZVL64 or S12ZVL128 provide 8x16 bit PWM channels but simple PWM.
Best regards,
Ladislav
不是自带六路PWM输出么 build in 6 channel PWM module
Doesn't it come with six PWM outputs? build in 6 channel PWM module