是否有mc9s12zvc系列can传输层驱动软件包?do we have Can transport layer protocol driver package for mc9s12zvc series ?Like lin NCFtool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

是否有mc9s12zvc系列can传输层驱动软件包?do we have Can transport layer protocol driver package for mc9s12zvc series ?Like lin NCFtool

741 Views
wangjiajie
Contributor III

zvc系列有没有传输层支持包?可有给个链接?

Do we have Can transport layer protocol driver package for mc9s12zvc series?

0 Kudos
2 Replies

451 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

No, there is no such a driver available.

The CAN module on S12Z derivatives is the same as older S12(woman). So, there shouldn't be any problem with implementing any CAN example designed for older S12(X) platforms. See for example:   

https://community.nxp.com/docs/DOC-93792

or

https://community.nxp.com/docs/DOC-329209

There is also CAN driver for S12XE and S12G devices.

You can use it as an development platform for S12Z or you can try to port it to this device changing addresses of the registers.

http://www.nxp.com/files/microcontrollers/software/device_drivers/MSCAN_S12_DEVD.zip.

Best regards,

Ladislav

0 Kudos

451 Views
wangjiajie
Contributor III

Thank you .

0 Kudos