Large custom NFC tags / antennas

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Large custom NFC tags / antennas

1,365件の閲覧回数
shanehill00
Contributor I

Currently, I am doing research, assessing feasibility and building a prototype of an NFC based product. I am discovering that the form factor for commonly available NFC tags are not going to meet my needs. So I need to start looking at something custom.

I am not an expert in the NFC field and I am still in early stages of research but I am quite serious about getting this done. Also, I have made prototypes that do work but like I mentioned above, the commonly available tags will not meet my form factor requirements.

The basic parameters of my needs are as follows:

1) Need to be able to operate on carbon fiber and metal (ferrite backed tags work in my testing)

2) I need the tag/antenna to operate over a large field. I am currently working with antennas of 45mm x 100mm

3) Ultimately, the tags will be inlaid into vinyl sheets 10-12 mils thick

Can someone help me understand how I would go about getting tags that fit the above requirements?

ラベル(1)
0 件の賞賛
0 返答(返信)