We have a custom card with LS1046A Processor. This is the UART log. I am not able login as root and it is not taking ifconfig command . Kindly help.
Where did you get the SD card image being used?
Please try pre-built composite firmware image for LS1046ARDB from:
https://lsdk.github.io/components.html
section LSDK IMAGES
"root" is default Linux login.
It should be active if not explicitly changed.
Try to erase SD card, deploy composite firmware image and boot.
The composite firmware with tiny yocto linux works fine.
These are the commands am giving to generate bootpartititon and rootfs after changing dts files in Linux.
flex-builder -c linux -a arm64
flex-builder -i mklinux -r ubuntu
flex-builder -i mkrfs -a arm64
flex-builder -i merge-component -a arm64
flex-builder -i packrfs -a arm64
flex-builder -i mkbootpartition -a arm64