Hi All,
I was trying to run qemu for QorIQ-SDK-V1.6-20140619 for t1024 processors and get error as below
(qemu) Trying to write invalid spr 532 (0x214) at c0001c94
The command which I run for running qemu is given below
~//QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/sysroots/x86_64-linux/usr/bin/qemu-system-ppc -nographic -M ppce500 -kernel /home/abhinav/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/deploy/images/t1040rdb/uImage -initrd /home/abhinav/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/deploy/images/t1040rdb/fsl-image-minimal-t1040rdb-20141222103228.rootfs.ext2.gz -append "root=dev/vda1 rw console=ttyS0,115200" -serial tcp::4444,server,nowait -smp 2
QEMU 1.7.0 monitor - type 'help' for more information
(qemu) Trying to write invalid spr 532 (0x214) at c0001c94
qemu: terminating on signal 2
Also when I tried with -enable-kvm I get below errors
~//QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/sysroots/x86_64-linux/usr/bin/qemu-system-ppc -enable-kvm -nographic -M ppce500 -kernel /home/abhinav/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/deploy/images/t1040rdb/uImage -initrd /home/abhinav/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/deploy/images/t1040rdb/fsl-image-minimal-t1040rdb-20141222103228.rootfs.ext2.gz -append "root=dev/ram rw console=ttyS0,115200" -serial tcp::4444,server,nowait -smp 2
KVM not supported for this target
"kvm" accelerator does not exist.
No accelerator found!
While building images using bitbake it gives below output
Build Configuration:
BB_VERSION = "1.22.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "CentOS-7.0.1406"
TARGET_SYS = "powerpc-fsl-linux"
MACHINE = "t1040rdb"
DISTRO = "fsl-networking"
DISTRO_VERSION = "1.6"
TUNE_FEATURES = "m32 fpu-hard e5500"
TARGET_FPU = "hard"
meta
meta-yocto
meta-yocto-bsp = "(detachedfromfsl-sdk-v1.6):0d2ce44c2b0f8cc9699e30cca2c24655be89d58b"
meta-fsl-ppc = "(detachedfromfsl-sdk-v1.6):6cf59d9de63a9fc5f8942c0d10c622898f4315ce"
meta-fsl-ppc-toolchain = "(detachedfromfsl-sdk-v1.6):a546e42f86e7d57de19e27907365d170b13fc18f"
meta-fsl-networking
meta-fsl-networking = "(detachedfrom8dec9c6):8dec9c690188cce5305ef5055f91e5cfa35c63f4"
meta-virtualization
meta-virtualization = "(detachedfromfsl-sdk-v1.6):8044073f63a0d99541a43ac5f2f6d789f94c7c7c"
meta-oe
meta-networking
meta-webserver
meta-ruby
meta-filesystems = "(detachedfromfsl-sdk-v1.6):b86007f742a1b829ccc8d76e485bb3f789cefaa4"
meta-java = "(detachedfromfsl-sdk-v1.6):d01f7d39e513790ddce20e6724723722119a3700"
meta-openstack
meta-openstack-compute-deploy
meta-openstack-controller-deploy
meta-openstack-qemu = "(detachedfromfsl-sdk-v1.6):f627404399a134672e0b5e26a0d9b794a6f8adf4"
So any thoughts to fix this issue.
Thanks,
Abhinav
已解决! 转到解答。
SPR 532 is IVOR36 (Processor Doorbell). When not using KVM, the default CPU for ppce500 is e500v2, which does not implement doorbells. You need to make sure the QEMU machine model matches what the OS you're trying to run expects. You can use the -cpu option to specify the CPU type -- for t1024 (or t1040), this should be e5500 and you should be using qemu-system-ppc64.
As for KVM, that is virtualization, not emulation. You need to be running on a PPC of the same type as you want the guest to see. From the path to the binary I can see that you're running this on an x86 host.
SPR 532 is IVOR36 (Processor Doorbell). When not using KVM, the default CPU for ppce500 is e500v2, which does not implement doorbells. You need to make sure the QEMU machine model matches what the OS you're trying to run expects. You can use the -cpu option to specify the CPU type -- for t1024 (or t1040), this should be e5500 and you should be using qemu-system-ppc64.
As for KVM, that is virtualization, not emulation. You need to be running on a PPC of the same type as you want the guest to see. From the path to the binary I can see that you're running this on an x86 host.
Hi,
Just an query as above answer helped and I was able to run the QEMU. But whenever I tried passing -enable-kvm (as refered in the documentations also http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F2888263.html ) I always get error as below
KVM not supported for this target
"kvm" accelerator does not exist.
No accelerator found!
So when this option can be used and if not then where I can find proper arguments need to be used as part of the stuff.
Thanks,
Abhinav
Again, KVM is for virtualization, not emulation. If you want to use KVM with an e5500 VM, you need to be running on an e5500 host. If you are wanting to emulate a PPC on an x86 host, you cannot use KVM. What host are you running on, and what type of guest are you trying to create?