qemu: Unsupported syscall: 277

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qemu: Unsupported syscall: 277

2,696 Views
tedlin
Contributor I

Hi 

i follow LSDK-KC-REV18.06.pdf to build up LS1043A's linux system.

i got a error message "qemu: Unsupported syscall: 277" when i use command

"flex-builder -i mkrfs -a arm64". the below is info. could you let me know what problem is it thanks?

Ted Lin

pastedImage_1.png

0 Kudos
Reply
1 Reply

1,597 Views
Pavel
NXP Employee
NXP Employee

Use Ubuntu 18.04 64bit version for SDK 18.06 building. There are no errors for this command if this Ubuntu is used.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply