Hello,I write a simple program to print time every 1ms.
#include <errno.h>
#include <signal.h>
#include <stdio.h>
#include <string.h>
#include <sys/resource.h>
#include <sys/time.h>
int main(void)
{
pid_t pid = getpid();
setpriority(PRIO_PROCESS, pid, -20);
while (1)
{
usleep(1000);
struct timeval t;
gettimeofday(&t, NULL);
printf("%u.%06u\n", t.tv_sec, t.tv_usec);
}
return 0;
}
while I get the following result.
......
1402463778.370107
1402463778.371202
1402463778.372297
1402463778.373393
1402463778.374487
1402463778.375582
1402463778.376677
1402463778.377772
1402463778.378893
1402463778.380010
1402463778.381105
1402463778.382199
1402463778.383293
1402463778.384388 ***********
1402463778.718214 ***********lost
1402463778.719311
1402463778.720407
1402463778.721502
1402463778.722597
1402463778.723691
1402463778.724786
1402463778.725896
1402463778.726992
......
about 300ms lost every 1s.Why?
Then I use setitimer() and pause()
struct itimerval tv;
tv.it_interval.tv_sec = 0;
tv.it_interval.tv_usec = 1000;
tv.it_value.tv_sec = 0;
tv.it_value.tv_usec = 1000;
I get the following result.
1402465124.8487241402465124.851723
1402465124.852722
1402465124.854723
1402465124.855724
1402465124.856722
1402465124.858724
1402465124.860722
1402465124.862724
1402465124.863722
1402465124.865724
1402465124.866724
1402465124.869723
1402465124.870721 ******
1402465124.872723 ******lost
1402465124.873724
1402465124.874722
1402465124.8767231402465124.879724 ******output overlap
1402465124.880723
1402465124.881721
1402465124.883724
1402465124.884741
1402465124.885722
1402465124.888721
1402465124.890723
1402465124.891724
1402465124.892722
1402465124.8947241402465124.897723
lost and output overlap.Why?
Thanks in advance for any help.
Look at the following pages about testing of this patch and priority changing for your task.
https://lwn.net/Articles/146861/
https://events.linuxfoundation.org/sites/events/files/slides/toyooka_LCJ2014_v10.pdf
http://people.redhat.com/williams/latency-howto/rt-latency-howto.txt
https://rt.wiki.kernel.org/index.php/RT_PREEMPT_HOWTO
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Linux is not real-time operating system.
See the following pages:
https://en.wikipedia.org/wiki/Real-time_operating_system
http://www.ni.com/white-paper/3938/en/
See the following pages about differences between Linux and real-time operating system:
http://www.nxp.com/files/soft_dev_tools/doc/white_paper/CWLNXRTOSWP.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------