ls1088ardb, kernel 5.4, fitimage bootm hangs if RANDOMIZE_BASE disabled + symbol offset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1088ardb, kernel 5.4, fitimage bootm hangs if RANDOMIZE_BASE disabled + symbol offset

947 Views
mthenault
Contributor I

Hi,

On kernel 5.4 (yocto hardknott), bootm hangs after "starting kernel" if the kernel config RANDOMIZE_BASE is disabled.

The issue is that with RANDOMIZE_BASE enabled, even with the nokaslr kernel option, there is a offset of 0x188000 between the vmlinux symbols and the actual running kernel. This makes debugging / dump analyzing complicated and not future proof, especially that I didn't find where this 0x188000 comes from.

Thanks in advance for your help !

I am using the default yocto fitimage layout:

/dts-v1/;
/ {
description = "FIT Image";
#address-cells = <1>;
images {
kernel {
description = "Kernel";
data = /incbin/("vmlinux.bin");
type = "kernel";
arch = "arm64";
os = "linux";
compression = "none";
load = <0x80008000>;
entry = <0x80008000>;
hash {
algo = "sha1";
};
};
fdt {
description = "DTB";
data = /incbin/("fsl-ls1048a.dtb");
type = "flat_dt";
arch = "arm64";
compression = "none";
load = <0x90000000>;
hash {
algo = "sha1";
};
};
};
configurations {
default = "standard";
standard {
description = "Standard Boot";
kernel = "kernel";
fdt = "fdt";
hash {
algo = "sha1";
};
};
};
};

0 Kudos
Reply
3 Replies

903 Views
mthenault
Contributor I

The issue is that we want to use bootm, because we need fitimage support (we want to enable secure boot)

0 Kudos
Reply

854 Views
yipingwang
NXP TechSupport
NXP TechSupport

I have escalated this case to the SE team, please refer to the following update from them.

Since maybe it's uboot's issue introduced by customer's custom needs, we have no plan to fix it.

Tags (1)
0 Kudos
Reply

918 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following suggestion from the SE team.

Suggest customer use booti instead of bootm when disabling config RANDOMIZE_BASE. Refer the following link for details.

https://www.mail-archive.com/u-boot@lists.denx.de/msg411672.html

0 Kudos
Reply