Hi,
I have a issue with the generation of MPPrivK and MPPubK from kernel space. The part of my code is below.
#define STD_BUF_SZ<---->256
#define OP_TYPE_SHIFT<-><------>24
#define OP_TYPE_MP_PUB_K_GENERATON<---->(0x06 << OP_TYPE_SHIFT)
#define OP_TYPE_MP_PRIV_K_GENERATON<--->(0x07 << OP_TYPE_SHIFT)
#define OP_PCLID_SHIFT<><------>16
#define OP_PCLID_PUBLICKEYPAIR<>(0x14 << OP_PCLID_SHIFT)
#define CMD_SHIFT<-----><------>27
#define CMD_OPERATION<-><------>(0x10 << CMD_SHIFT)
#define PDB_MP_CSEL_SHIFT<----->17
#define PDB_MP_CSEL_P256<------>0x3 << PDB_MP_CSEL_SHIFT<------>/* P-256 */
#define PDB_MP_CSEL_P384<------>0x4 << PDB_MP_CSEL_SHIFT<------>/* P-384 */
#define PDB_MP_CSEL_P521<------>0x5 << PDB_MP_CSEL_SHIFT<------>/* P-521 */
struct job_result {
<------>int error;
<------>struct completion completion;
};
struct pdb_mp_pub_k {
<------>u32 <--><------>pdb_hdr;
<------>#define PDB_MP_PUB_K_SGF_SHIFT<>31
<------>dma_addr_t <--->dma_pkey;<----->/* Pointer to Wx,y (public key) */
};
struct pdb_mp_priv_k {
<------>u32 <--><------>pdb_hdr;
<------>#define PDB_MP_PRIV_K_SGF_SHIFT>31
<------>dma_addr_t <--->dma_msg;<------>/* Pointer to m */
};
static void job_done(struct device *dev, u32 *desc, u32 err, void *context)
{
<------>struct job_result *res = context;
<------>if (err)
<------><------>caam_jr_strstatus(dev, err);
<------>res->error = err;
<------>complete(&res->completion);
}
static int get_pub_key(struct device *jr_dev, u8 *outbuf)
{
<------>u32 *desc;
<------>u8 *pkey;
<------>int ret = -ENOMEM;
<------>struct job_result testres;
<------>struct pdb_mp_pub_k *pdb;
<------>pdb = kmalloc(sizeof(struct pdb_mp_pub_k), GFP_KERNEL | GFP_DMA);
<------>if (!pdb) {
<------><------>dev_err(jr_dev, "unable to allocate pdb memory\n");
<------><------>goto out_free;
<------>}
<------>pdb->pdb_hdr |= PDB_MP_CSEL_P256;
<------>pdb->pdb_hdr |= (1<<PDB_MP_PRIV_K_SGF_SHIFT);
<------>desc = kmalloc(MAX_CAAM_DESCSIZE, GFP_KERNEL | GFP_DMA);
<------>if (!desc) {
<------><------>dev_err(jr_dev, "unable to allocate desc memory\n");
<------><------>goto out_free;
<------>}
<------>memset(desc, 0, MAX_CAAM_DESCSIZE);
<------>pkey = kmalloc((STD_BUF_SZ*2), GFP_KERNEL | GFP_DMA);
<------>if(!pkey) {
<------><------>dev_err(jr_dev, "unable to allocate memory for public key\n");
<------><------>goto out_free;
<------>}
<------>memset(pkey, 0, (STD_BUF_SZ*2));
<------>pdb->dma_pkey = dma_map_single(jr_dev, (void *)pkey, STD_BUF_SZ*2,
<------><------><------><------> DMA_TO_DEVICE);
<------>if (dma_mapping_error(jr_dev, pdb->dma_pkey)) {
<------><------>dev_err(jr_dev, "unable to map public key output memory\n");
<------><------>goto out_free;
<------>}
<------>init_job_desc_pdb(desc, 0, sizeof(struct pdb_mp_pub_k));
<------>dma_sync_single_for_device(jr_dev, pdb->dma_pkey, STD_BUF_SZ*2, DMA_TO_DEVICE);
<------>append_cmd(desc, pdb->pdb_hdr);
<------>append_ptr(desc, pdb->dma_pkey);
<------>append_operation(desc, CMD_OPERATION | OP_TYPE_MP_PUB_K_GENERATON \
<------><------><------><------>| OP_PCLID_PUBLICKEYPAIR);
<------>testres.error = 0;
<------>init_completion(&testres.completion);
<------>ret = caam_jr_enqueue(jr_dev, desc, job_done, &testres);
<------>if (!ret) {
<------><------>// in progress
<------><------>dev_info(jr_dev, "job ring return %d\n", testres.error);
<------><------>dma_sync_single_for_cpu(jr_dev, pdb->dma_pkey, STD_BUF_SZ*2, DMA_FROM_DEVICE);
<------><------>wait_for_completion(&testres.completion);
<------><------>ret = testres.error;
<------><------>if (ret) {
<------><------><------><------>goto out_free;
<------><------><------>}
<------>}
<------>dma_unmap_single(jr_dev, pdb->dma_pkey, STD_BUF_SZ*2, DMA_FROM_DEVICE);
<------>memcpy(outbuf, pkey, STD_BUF_SZ*2);
out_free:
<------>kfree(pkey);
<------>kfree(desc);
<------>return ret;
}
It doesn't return any errors. But outbuf is empty.
Advise me please right data flow for MP keys generation.
Thanks.
Best regards,
Andrey.
Please refer to the attached MP key generate code in u-boot.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------