ls1046 : fm1-mac5 and switch ports cannot auto-negotiation to 1000base-Tx mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1046 : fm1-mac5 and switch ports cannot auto-negotiation to 1000base-Tx mode

563 Views
hongyuanz
Contributor IV

The first power on is normal, reboot ls1046 fails to auto-negotiate  to 100base-Tx mode

 

0 Kudos
1 Reply

469 Views
yipingwang
NXP TechSupport
NXP TechSupport

I believe that the mode you are referring is 1000base-KX and not 1000base-TX.
Does it mean, that you are connecting it to an external switch on 100base-KX?
If that is the case, then I would recommend disabling the auto-negotiation (AN) mode.

Additionally, on Linux, you have to use the "fixed link driver" whenever the auto-negotiation mode is disabled.

0 Kudos