ls1043 sd boot,no log output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1043 sd boot,no log output

1,056 Views
412149526
Contributor I

We customized the ls1043 board and boot from the sd card. Now plug in the sd card, but there is no output from the serial port, we have checked and the voltage and power-on sequence are normal, can there be other places to check

Tags (1)
0 Kudos
Reply
5 Replies

1,012 Views
ufedor
NXP Employee
NXP Employee

Use a digital scope and check:

1) RCW is read from the SD card

2) RESET_REQ_B is not asserted after the RCW readout

0 Kudos
Reply

1,012 Views
412149526
Contributor I

Whether the serder configuration is incorrect will also cause problems with startup

0 Kudos
Reply

1,012 Views
ufedor
NXP Employee
NXP Employee

Incorrect SerDes configuration will initiate RESET_REQ_B assertion.

0 Kudos
Reply

1,012 Views
412149526
Contributor I

How to check that the SerDes configuration is correct, which aspects need to be checked? Thank you!

0 Kudos
Reply

1,012 Views
ufedor
NXP Employee
NXP Employee

It is needed to refer to the QorIQ LS1043A Reference Manual, Table 33-1. Supported SerDes options and Table 33-4. Valid SerDes RCW Encodings and Reference Clocks.

0 Kudos
Reply