ls1021/2 CAN bus issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1021/2 CAN bus issue

687件の閲覧回数
liyingchun
Contributor I

Hi

ls1021/2 have 4 can bus controller.  I want to know that if the lsl02x cpu support wake up from can bus?

タグ(2)
0 件の賞賛
1 返信

524件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello li yingchun,

According to the LS1021ARM, there are five basic mechanisms to wake up the chip from deep sleep:

• Ethernet event

• UART Activity

• I2C Bus Activity such as reception of packet.

• Internal timer event

• External pin event

So I am afraid no.

Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛