ls1012 ieee1588

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1012 ieee1588

779件の閲覧回数
lizuobin
Contributor II

Hello, friend.

In ls1012 or ls1043 platform,How to configure device tree for  etsec-ptp ?

ptp_clock@2d10e00 {
   compatible = "fsl,etsec-ptp";
   reg = <0x0 0x2d10e00 0x0 0xb0>;
   interrupts = <GIC_SPI 173 IRQ_TYPE_LEVEL_HIGH>;
   fsl,tclk-period = <5>;
   fsl,tmr-prsc = <2>;
   fsl,tmr-add = <0xaaaaaaab>;
   fsl,tmr-fiper1 = <999999990>;

   fsl,tmr-fiper2 = <99990>;
   fsl,max-adj = <499999999>;

};

ptp_timer0: ptp-timer@fe000 {
  compatible = "fsl,fman-ptp-timer", "fsl,fman-rtc";
  reg = <0xfe000 0x1000>;
};

Configurations can be found in lsdk18.03, but they are not applicable to ls1012 or ls1043 platforms.

タグ(4)
0 件の賞賛
返信
1 返信

647件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Table 4 of NXP LSDK 18.06 documentation:

https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV18.06.pdf

 

This Table shows that IEEE1588, PTPD is not supported for the LS1012a.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------