gianfar non dpaa - git.freescale.com qoriq SDK 1.2 with patches vs meta-fsl-ppc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gianfar non dpaa - git.freescale.com qoriq SDK 1.2 with patches vs meta-fsl-ppc

514件の閲覧回数
maheshbalasubr1
Contributor II

Hi,

Sorry to repeat variant of git.freescale.com queries. 

#1. For BSC9132, if we want to regenerate exact replica of below old repository url 

http://git.freescale.com/git/cgit.cgi/ppc/sdk/linux.git/?h=sdk-v1.2.x

will cloning the meta-fsl-ppc tag fsl-sdk-v1.2.1 and including it SDK 1.2 build good enough?  

https://source.codeaurora.org/external/qoriq/qoriq-yocto-sdk/meta-fsl-ppc/

Checking this to trace out a very old vendor implementation differences.

#2. "meta-fsl-ppc" layer seems to be frozen around 2015, to port gianfar(non DPAA) driver framework to the latest optimized version is SDK 1.6 a good choice?

Thanks

0 件の賞賛
1 返信

501件の閲覧回数
bpe
NXP Employee
NXP Employee

You are asking about very old SDK releases for which we can provide only very
limited support. The final SDK version that supports BSC9132 is 1.9. If you
wish to use code that was tested on your processor, stay with that SDK.
This recommendation applies to gianfar/eTSEC driver as well. It is not in
active development anymore and source code repositories for it are no longer
available online. The source code of the software that comprises the SDK can
be found it's source DVD image.

 

Best Regards,
Platon

0 件の賞賛