fsl-image-minimal start can't mount rootfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fsl-image-minimal start can't mount rootfs

1,188件の閲覧回数
biqierben
Contributor I

I had built the fsl-image-minimal -m ls1021atwr in sdk2.0-yocto, and deploy to the TWR-LS1021A-PC

after boot Uboot and kernal, the rootfs can't mount to ram, what happend?

what can i do ?

please help me!

for start infomation as follow:

U-Boot 2016.092.0+ga06b209 (May 15 2018 - 19:21:50 -0700)

CPU: Freescale LayerScape LS1021E, Version: 2.0, (0x87081120)
Clock Configuration:
CPU0(ARMV7):1000 MHz,
Bus:300 MHz, DDR:800 MHz (1600 MT/s data rate),
Reset Configuration Word (RCW):
00000000: 0608000a 00000000 00000000 00000000
00000010: 30000000 00007900 e0025a00 21046000
00000020: 00000000 00000000 00000000 18000000
00000030: 00080000 481b7340 00000000 00000000
Model: LS1021A TWR Board
Board: LS1021ATWR
CPLD: V3.3
PCBA: V2.0
VBank: 1
I2C: ready
DRAM: 1 GiB
Using SERDES1 Protocol: 48 (0x30)
Not a microcode
Flash: 128 MiB
MMC: FSL_SDHC: 0
EEPROM: NXID v1
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated
SATA link 0 timeout.
AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc
Found 0 device(s).
SCSI: Net: eTSEC1 is in sgmii mode.
eTSEC2 is in sgmii mode.
PCIe0: pcie@3400000 Root Complex: x1 gen1
PCIe1: pcie@3500000 disabled
eTSEC1 [PRIME], eTSEC2, eTSEC3

=> setenv bootargs root=/dev/ram rw console=ttyS0,115200 ramdisk_size=0x40000000
=> saveenv
Saving Environment to Flash...
Un-Protected 1 sectors
Erasing Flash...
. done
Erased 1 sectors
Writing to Flash... 9....8....7....6....5....4....3....2....1....done
Protected 1 sectors
=> pri
baudrate=115200
bootargs=root=/dev/ram rw console=ttyS0,115200 ramdisk_size=0x40000000
bootdelay=3
eth1addr=00:04:9F:05:3B:98
eth2addr=00:04:9F:05:3B:99
ethact=eTSEC1
ethaddr=00:04:9F:05:3B:97
ethprime=eTSEC1
fdt_high=0xa0000000
fdtcontroladdr=bef0dd34
initrd_high=0xa0000000
ipaddr=192.168.1.100
scsidevs=0
serverip=192.168.1.101

Environment size: 360/131068 bytes
=> tftp 0x83000000 uImage-ls1021atwr.bin
Speed: 1000, full duplex
Using eTSEC1 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.100
Filename 'uImage-ls1021atwr.bin'.
Load address: 0x83000000
Loading: #################################################################
#################################################################
#################################################################
#############################################
2.8 MiB/s
done
Bytes transferred = 3518216 (35af08 hex)
CACHE: Misaligned operation at range [83000000, 8335af08]
=> tftp 0x88000000 fsl-image-minimal-ls1021atwr.ext2.gz.u-boot
Speed: 1000, full duplex
Using eTSEC1 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.100
Filename 'fsl-image-minimal-ls1021atwr.ext2.gz.u-boot'.
Load address: 0x88000000
Loading: #################################################################
#################################################################
#################################################################
########################################################
2.9 MiB/s
done
Bytes transferred = 3677901 (381ecd hex)
CACHE: Misaligned operation at range [88000000, 88381ecd]
=> tftp 0x8f000000 uImage-ls1021a-twr.dtb
Speed: 1000, full duplex
Using eTSEC1 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.100
Filename 'uImage-ls1021a-twr.dtb'.
Load address: 0x8f000000
Loading: ##
361.3 KiB/s
done
Bytes transferred = 21482 (53ea hex)
CACHE: Misaligned operation at range [8f000000, 8f0053ea]
=> bootm 0x83000000 0x88000000 0x8f000000
## Booting kernel from Legacy Image at 83000000 ...
Image Name: Linux-4.1.35-rt41+g1ae843c
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3518152 Bytes = 3.4 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 88000000 ...
Image Name: fsl-image-minimal-ls1021atwr-201
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 3677837 Bytes = 3.5 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 8f000000
Booting using the fdt blob at 0x8f000000
Loading Kernel Image ... OK
Loading Ramdisk to 9fc7e000, end 9ffffe8d ... OK
Loading Device Tree to 9fc75000, end 9fc7d3e9 ... OK

Starting kernel ...

Booting Linux on physical CPU 0xf00
Linux version 4.1.35-rt41+g1ae843c (ylban@ubuntu) (gcc version 4.9.3 20150311 (prerelease) (Linaro GCC 4.9-2015.03) ) #1 SMP Wed May 16 23:09:35 PDT 2018
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=70c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: LS1021A TWR Board
Forcing write-allocate cache policy for SMP
Memory policy: Data cache writealloc
psci: probing for conduit method from DT.
psci: PSCIv1.0 detected in firmware.
psci: Using standard PSCI v0.2 function IDs
PERCPU: Embedded 12 pages/cpu @bf7cd000 s16640 r8192 d24320 u49152
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: root=/dev/ram rw console=ttyS0,115200 ramdisk_size=0x40000000
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1029588K/1048576K available (3703K kernel code, 226K rwdata, 1764K rodata, 256K init, 210K bss, 18988K reserved, 0K cma-reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f800000 - 0x7fe00000 ( 6 MB)
.text : 0x80008000 - 0x8055f1f0 (5469 kB)
.init : 0x80560000 - 0x805a0000 ( 256 kB)
.data : 0x805a0000 - 0x805d8868 ( 227 kB)
.bss : 0x805db000 - 0x8060f824 ( 211 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Hierarchical RCU implementation.
Additional per-CPU info printed with stalls.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
Architected cp15 timer(s) running at 12.50MHz (phys).
clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049cda, max_idle_ns: 440795202628 ns
sched_clock: 56 bits at 12MHz, resolution 80ns, wraps every 4398046511080ns
Switching to timer-based delay loop, resolution 80ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 25.00 BogoMIPS (lpj=125000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
CPU0: update cpu_capacity 1024
CPU0: thread -1, cpu 0, socket 15, mpidr 80000f00
Setting up static identity map for 0x80008280 - 0x800082e4
CPU1: update cpu_capacity 1024
CPU1: thread -1, cpu 1, socket 15, mpidr 80000f01
Brought up 2 CPUs
SMP: Total of 2 processors activated (50.00 BogoMIPS).
CPU: All CPU(s) started in HYP mode.
CPU: Virtualization extensions available.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
Machine: LS1021A TWR Board
SoC family: QorIQ LS1021A
SoC ID: svr:0x87081120, Revision: 2.0
irq: no irq domain found for /soc/uqe@2400000/qeic@80 !
irq: no irq domain found for /soc/uqe@2400000/qeic@80 !
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
register e1000-wakeup irq error, ret = -22
Serial: AMBA PL011 UART driver
RCPM: layerscape_rcpm_init: Fail to get "fsl,#rcpm-wakeup-cells".
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource arch_sys_counter
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 3592K (9fc7e000 - a0000000)
kvm [1]: interrupt-controller@1404000 IRQ22
kvm [1]: timer IRQ18
kvm [1]: Hyp mode initialized successfully
CPU PMU: Failed to parse /pmu/interrupt-affinity[0]
hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available
futex hash table entries: 512 (order: 3, 32768 bytes)
HugeTLB registered 2 MB page size, pre-allocated 0 pages
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
ls-scfg-msi soc:msi-controller: ibs_shift:3 msir_irqs:32 msir_base:0x4
Find msi-controller /soc/msi-controller
PCI host bridge /soc/pcie@3400000 ranges:
IO 0x4000010000..0x400001ffff -> 0x00000000
MEM 0x4040000000..0x407fffffff -> 0x40000000
layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [bus 00-ff]
pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
pci_bus 0000:00: root bus resource [mem 0x4040000000-0x407fffffff] (bus address [0x40000000-0x7fffffff])
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 8: assigned [mem 0x4040000000-0x40400fffff]
pci 0000:00:00.0: BAR 6: assigned [mem 0x4040100000-0x40401007ff pref]
pci 0000:01:00.0: BAR 0: assigned [mem 0x4040000000-0x404001ffff 64bit]
pci 0000:01:00.0: BAR 6: assigned [mem 0x4040020000-0x404002ffff pref]
pci 0000:00:00.0: PCI bridge to [bus 01]
pci 0000:00:00.0: bridge window [mem 0x4040000000-0x40400fffff]
sii902x: probe of 1-0039 failed with error -1
Console: switching to colour frame buffer device 60x34
fb0: fb device registered successfully.
fb1: fb device registered successfully.
fb2: fb device registered successfully.
fb3: fb device registered successfully.
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
console [ttyS0] disabled
21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 31, base_baud = 9375000) is a 16550A
console [ttyS0] enabled
21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 31, base_baud = 9375000) is a 16550A
2950000.serial: ttyLP0 at MMIO 0x2950000 (irq = 37, base_baud = 6250000) is a FSL_LPUART
fsl-lpuart 2950000.serial: DMA tx channel request failed, operating without tx DMA
fsl-lpuart 2950000.serial: DMA rx channel request failed, operating without rx DMA
brd: module loaded
loop: module loaded
ahci-qoriq 3200000.sata: AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl platform mode
ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc
ahci-qoriq 3200000.sata: port 0 is not capable of FBS
scsi host0: ahci-qoriq
ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 25
60000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00227e
Amd/Fujitsu Extended Query Table at 0x0040
Amd/Fujitsu Extended Query version 1.3.
number of CFI chips: 1
10 ofpart partitions found on MTD device 60000000.nor
Creating 10 MTD partitions on "60000000.nor":
0x000000000000-0x000000020000 : "NOR bank0 RCW Image"
0x000000100000-0x000000200000 : "NOR bank0 u-boot Image"
0x000000200000-0x000000300000 : "NOR bank0 DTB Image"
0x000000300000-0x000000a00000 : "NOR bank0 Linux Kernel Image"
0x000000a00000-0x000004000000 : "NOR bank0 Ramdisk Root File System Image"
0x000004000000-0x000004020000 : "NOR bank4 RCW Image"
0x000004100000-0x000004200000 : "NOR bank4 u-boot Image"
0x000004200000-0x000004300000 : "NOR bank4 DTB Image"
0x000004300000-0x000004a00000 : "NOR bank4 Linux Kernel Image"
0x000004a00000-0x000008000000 : "NOR bank4 Ramdisk Root File System Image"
m25p80 spi0.0: unrecognized JEDEC id bytes: ff, ff, ff
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
CAN device driver interface
2a70000.can supply xceiver not found, using dummy regulator
flexcan 2a70000.can: device registered (reg_base=c08ba000, irq=46)
2a80000.can supply xceiver not found, using dummy regulator
flexcan 2a80000.can: device registered (reg_base=c08bc000, irq=47)
libphy: Freescale PowerQUICC MII Bus: probed
fsl-gianfar soc:ethernet@2d10000: enabled errata workarounds, flags: 0x4
fsl-gianfar soc:ethernet@2d10000 eth0: mac: 00:04:9f:05:3b:97
fsl-gianfar soc:ethernet@2d10000 eth0: Running with NAPI enabled
fsl-gianfar soc:ethernet@2d10000 eth0: RX BD ring size for Q[0]: 256
fsl-gianfar soc:ethernet@2d10000 eth0: RX BD ring size for Q[1]: 256
fsl-gianfar soc:ethernet@2d10000 eth0: TX BD ring size for Q[0]: 256
fsl-gianfar soc:ethernet@2d10000 eth0: TX BD ring size for Q[1]: 256
fsl-gianfar soc:ethernet@2d50000: enabled errata workarounds, flags: 0x4
fsl-gianfar soc:ethernet@2d50000 eth1: mac: 00:04:9f:05:3b:98
fsl-gianfar soc:ethernet@2d50000 eth1: Running with NAPI enabled
fsl-gianfar soc:ethernet@2d50000 eth1: RX BD ring size for Q[0]: 256
fsl-gianfar soc:ethernet@2d50000 eth1: RX BD ring size for Q[1]: 256
fsl-gianfar soc:ethernet@2d50000 eth1: TX BD ring size for Q[0]: 256
fsl-gianfar soc:ethernet@2d50000 eth1: TX BD ring size for Q[1]: 256
fsl-gianfar soc:ethernet@2d90000: enabled errata workarounds, flags: 0x4
fsl-gianfar soc:ethernet@2d90000 eth2: mac: 00:04:9f:05:3b:99
fsl-gianfar soc:ethernet@2d90000 eth2: Running with NAPI enabled
fsl-gianfar soc:ethernet@2d90000 eth2: RX BD ring size for Q[0]: 256
fsl-gianfar soc:ethernet@2d90000 eth2: RX BD ring size for Q[1]: 256
fsl-gianfar soc:ethernet@2d90000 eth2: TX BD ring size for Q[0]: 256
fsl-gianfar soc:ethernet@2d90000 eth2: TX BD ring size for Q[1]: 256
pps pps0: new PPS source ptp0
e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k
e1000e: Copyright(c) 1999 - 2014 Intel Corporation.
ata1: SATA link down (SStatus 0 SControl 300)
xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66c hci version 0x100 quirks 0x00010010
xhci-hcd xhci-hcd.0.auto: irq 49, io mem 0x03100000
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
usbcore: registered new interface driver usb-storage
mousedev: PS/2 mouse device common for all mice
i2c /dev entries driver
ina2xx 0-0040: power monitor ina220 (Rshunt = 1000 uOhm)
ina2xx 0-0041: power monitor ina220 (Rshunt = 1000 uOhm)
0-004c supply vcc not found, using dummy regulator
imx2-wdt 2ad0000.watchdog: timeout 60 sec (nowayout=0)
qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc 1560000.esdhc: No vmmc regulator found
sdhci-esdhc 1560000.esdhc: No vqmmc regulator found
mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit
caam 1700000.crypto: Instantiated RNG4 SH1
caam 1700000.crypto: device ID = 0x0a14030000000000 (Era 7)
caam 1700000.crypto: job rings = 4, qi = 0
caam algorithms registered in /proc/crypto
caam_jr 1710000.jr: registering rng-caam
caam 1700000.crypto: fsl,sec-v5.0 algorithms registered in /proc/crypto
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
sgtl5000 1-000a: sgtl5000 revision 0x11
oprofile: using timer interrupt.
Initializing XFRM netlink socket
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
Key type dns_resolver registered
Registering SWP/SWPB emulation handler
sgtl5000 1-000a: Using internal LDO instead of VDDD
asoc-simple-card sound: sgtl5000 <-> 2b50000.sai mapping ok
hctosys: unable to open rtc device (rtc0)
ALSA device list:
#0: 2b50000.sai-sgtl5000
usb 1-1: new high-speed USB device number 2 using xhci-hcd
RAMDISK: gzip image found at block 0
RAMDISK: incomplete write (-28 != 32768)
write error
List of all partitions:
0100 9223372035781033984 ram0 (driver?)
0101 9223372035781033984 ram1 (driver?)
0102 9223372035781033984 ram2 (driver?)
0103 9223372035781033984 ram3 (driver?)
0104 9223372035781033984 ram4 (driver?)
0105 9223372035781033984 ram5 (driver?)
0106 9223372035781033984 ram6 (driver?)
0107 9223372035781033984 ram7 (driver?)
1f00 128 mtdblock0 (driver?)
1f01 1024 mtdblock1 (driver?)
1f02 1024 mtdblock2 (driver?)
1f03 7168 mtdblock3 (driver?)
1f04 55296 mtdblock4 (driver?)
1f05 128 mtdblock5 (driver?)
1f06 1024 mtdblock6 (driver?)
1f07 1024 mtdblock7 (driver?)
1f08 7168 mtdblock8 (driver?)
1f09 55296 mtdblock9 (driver?)
No filesystem could mount root, tried: ext3 ext2 ext4 vfat msdos
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)
CPU: 1 PID: 1 Comm: swapper/0 Not tainted 4.1.35-rt41+g1ae843c #1
Hardware name: Freescale LS1021A
[<8001d2bd>] (unwind_backtrace) from [<8001ae53>] (show_stack+0xb/0xc)
[<8001ae53>] (show_stack) from [<80372dd3>] (dump_stack+0x5b/0x74)
[<80372dd3>] (dump_stack) from [<803709c9>] (panic+0x55/0x158)
[<803709c9>] (panic) from [<80560d15>] (mount_block_root+0x131/0x16c)
[<80560d15>] (mount_block_root) from [<80560e7b>] (mount_root+0x87/0xa8)
[<80560e7b>] (mount_root) from [<80560f5d>] (prepare_namespace+0xc1/0x114)
[<80560f5d>] (prepare_namespace) from [<80560a8d>] (kernel_init_freeable+0x111/0x158)
[<80560a8d>] (kernel_init_freeable) from [<8036f76f>] (kernel_init+0x7/0x94)
[<8036f76f>] (kernel_init) from [<80018b41>] (ret_from_fork+0x11/0x30)
CPU0: stopping
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.1.35-rt41+g1ae843c #1
Hardware name: Freescale LS1021A
[<8001d2bd>] (unwind_backtrace) from [<8001ae53>] (show_stack+0xb/0xc)
[<8001ae53>] (show_stack) from [<80372dd3>] (dump_stack+0x5b/0x74)
[<80372dd3>] (dump_stack) from [<8001c985>] (handle_IPI+0x81/0xf4)
[<8001c985>] (handle_IPI) from [<8000933f>] (gic_handle_irq+0x3b/0x44)
[<8000933f>] (gic_handle_irq) from [<80375fdb>] (__irq_svc+0x3b/0x5c)
Exception stack(0x805a1f58 to 0x805a1fa0)
1f40: 00000001 00000000
1f60: 00000000 80023a41 805a0000 00000000 00000001 00000000 805a1fa8 8059a41c
1f80: 8058aa30 00000000 805a2180 805a1fa0 80019491 80019492 40000133 ffffffff
[<80375fdb>] (__irq_svc) from [<80019492>] (arch_cpu_idle+0x14/0x1e)
[<80019492>] (arch_cpu_idle) from [<8004e76f>] (cpu_startup_entry+0x173/0x1ac)
[<8004e76f>] (cpu_startup_entry) from [<80560913>] (start_kernel+0x273/0x2dc)
[<80560913>] (start_kernel) from [<8000808f>] (0x8000808f)
---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)

?????????????????????????????????????????????

0 件の賞賛
返信
1 返信

708件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello biqier ben,

Please download the pre-built image ISO QorIQ-SDK-V2.0-CORTEXA7-IMAGE-20160527-yocto.iso to check whether you could boot the target board successfully with image ls1021atwr/fsl-image-core-ls1021atwr.ext2.gz.u-boot.

If yes, there should be problem with the image fsl-image-minimal-ls1021atwr.ext2.gz.u-boot, which you built.

Please regenerate fsl-image-minimal ramdisk rootfs image with the following commands.

$ bitbake fsl-image-minimal -c cleansstate

$ bitbake fsl-image-minimal

Thanks,

Yiping

0 件の賞賛
返信