frdm-ls1012a-pa ppa

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

frdm-ls1012a-pa ppa

653 Views
mukunkong
Contributor I

I have a board frdm-ls1012a-pa,now,i need flash ppa firmware to QSPI flash,command `sf write 0x96000000 0x50000 $ppa_file_size` and reset board,but serial console print 

 Reset Configuration Word (RCW):
 00000000: 08000008 00000000 00000000 00000000
 00000010: 33050000 c000000c 40000000 00001800
 00000020: 00000000 00000000 00000000 000c4571
 00000030: 00000000 00c28120 00000096 00000000
 I2C: ready
 DRAM: 510 MiB

fsl-ppa: Bad firmware image (not a FIT image)
 fsl-ppa: error (-22)


 Using SERDES1 Protocol: 13061 (0x3305)
 SF: Detected S25FS512S_256K with page size 512 Bytes, erase size 128 KiB, total 64 MiB

Can you help me,thanks

0 Kudos
Reply
1 Reply

520 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello 穆 昆空,

PPA FIT image is at 0x4050_0000, offset 0x500000 on QSPI flash. Please refer to the following procedure.

=>tftp 0x80000000 ppa.itb

=>sf probe 0:0

=>sf erase 0x500000 +$filesize

=>sf write 0x80000000 0x500000 $filesize

=>reset


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply