decode MAS registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

decode MAS registers

2,473 Views
hv
Contributor II

I see these values in the MAS registers but not sure what they are telling me:

MAS0 = 0x00000001

MAS1 = 0x80000000

MAS2 = 0x291A0000

MAS3 = 0x00000000

Thanks!

10 Replies

2,282 Views
scottwood
NXP Employee
NXP Employee

You can find the description of the MAS registers in the EREF manual, or in the Power ISA 2.06.

The TLB entry described above is not valid for translation as all permission bits are clear.

0 Kudos

2,282 Views
hv
Contributor II

Thanks!

Does NV (Next Victim) = 1 indicates that I have a TLB miss?

Sorry but I'm new at this.

0 Kudos

2,282 Views
scottwood
NXP Employee
NXP Employee

No.  Taking a TLB error exception indicates you have a TLB miss.  When you've taken a TLB miss (or executed tlbsx or tlbre) NV will contain a suggestion for which ESEL to use.  Otherwise (including when taking an ISI/DSI exception, which is what you'd get with the TLB entry you showed), NV is undefined.

0 Kudos

2,282 Views
hv
Contributor II

Did I get an ISI/DSI exception because all the permission bits are clear?

“The TLB entry’s permission bits

(TLB[US,SX,UW,SW,UR,SR]) determine whether the operation should succeed. If permission is denied,

execution of the instruction is suppressed and an instruction or data storage interrupt occurs.”

0 Kudos

2,282 Views
scottwood
NXP Employee
NXP Employee

Yes, if you try to access an address whose TLB entry does not have the relevant permission bit set, you'll get an ISI or DSI.

0 Kudos

2,282 Views
hv
Contributor II

Hi Scott,

I’m working with a P2041RDB. I’m using uboot as a bootloader. Uboot sets up core 0 and holds other cores in spin loop.

Now I want to set up MMU for core 1 before I release it.

Here’s what I do to set up a mapping that maps addr 1:1 for 64M

// MAS0 = 0x10010000 (TLB1 is selected, IPROT = 1 and 1st entry)

lis r5,0x1003

ori r5,r5,0x0000

mtspr 624,r5

//MAS1 = 0xC0000800 (TSIZE = 64MB)

lis r5,0xC000

ori r5,r5,0x1800

mtspr 625,r5

// MAS2 = 0x00000210 (effective page number = 0 and effective address range = 0,

// share enabled is set and the page is set up as write-thru).

lis r5,0x0000

ori r5,r5,0x0210

mtspr 626,r5

// MAS3 = 0x00000015 (SX=1, SW=1, SR=1)

lis r5,0x0000

ori r5,r5,0x0015

mtspr 627,r5

tlbwe

msync

isync

Does that look correct? The code that I have that following this setup doesn’t work properly. So I just want to check and see if my setup was done correctly.

Thanks!

0 Kudos

2,282 Views
scottwood
NXP Employee
NXP Employee

You can't set up the MMU on core 1 before you release it.  You can only set up the MMU on cores you're already running on.  The U-boot spin table code will create a mapping for core 1 when it is released.  See the documentation of SIMA in ePAPR.

0 Kudos

2,282 Views
hv
Contributor II

I think I got a DSI based on these values:

PC: 0x000001C0

SRR0: 0x00006090

SRR1: 0x00000000

DEAR: 0x04000000

ESR: 0x00800000

I think the instruction that caused the DSI is this:

stw r3, 0(r11)

I saw this in the EREF:

Software can determine if the exception

occurred during a page table translation by examining ESR[PT] (or GESR[PT] <E.HV>).

I can’t tell what the ESR[PT] is telling me.

Thanks!

2,282 Views
scottwood
NXP Employee
NXP Employee

ESR[PT] indicates the fault was from a bad entry in a hardware page table (i.e. something pointed to by a TLB1 entry with the indirect bit set).  That bit is not set, so I'm not sure why you're asking about it.  The only bit set in ESR above is ESR[ST], which indicates that the access was a store rather than a load.

0 Kudos

2,282 Views
hv
Contributor II

So I didn’t have a TLB miss but an ISI/DSI exception. Correct?

FYI, I’m trying to set up MMU on core 1 of a P2041RDB by mimicking what u-boot did with core 0. I guess I didn’t do that correctly.

0 Kudos