can P2020 support eMMC 4.51 or eMMC 5.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can P2020 support eMMC 4.51 or eMMC 5.0?

1,476 Views
amirabbasshahva
Contributor I

 can P2020 support eMMC 4.51 or eMMC 5.0?

4 Replies

871 Views
toshiyukimaekaw
Contributor II

Thank you for sending your gracious response so promptly.
That is highly valuable information

0 Kudos

871 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Originally eMMC specifications besides of the physical factors are based on MMC rev 4.2 which is supported by the P2020 eSDHC. The new features introduced in the rev 4.3 to rev 4.5 and rev. 5 of the MMC specs are not supported. I have listened about the P2020 designs with eMMC 4.5. Typically, the eMMC is back compatible to the rev 4.2 MMC specs. To be sure you can ask eMMC producer if its eMMC device  is back compatible to the rev 4.2 MMC specs.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

871 Views
toshiyukimaekaw
Contributor II

Dear Serguei Podiatchev,

We have adopted QorIQ P1021/2010/2020 for our products.
And we connected between QorIQ and eMMC for boot device.
The eMMC 4.2 device supported by QorIQ is already discontinued.
We must change other eMMC device.

eMMC 4.2 added support for SPI mode. (old eMMC support SDR Mode only.)
However, since eMMC 4.3, support for SPI mode has been removed again.
For this reason, eMMC manufacturers replied that eMMC 5.0 is not back compatible to the rev 4.2 MMC specs.

We have question for you.
Does QorIQ P1021/2010/2020 require SPI mode at boot time?
Or, does QorIQ P1021/2010/2020 require SDR mode at boot time?

Thank you for your time and consideration.

Best Regards,
Toshiyuki Maekawa,
Advanet Inc.

0 Kudos

871 Views
r8070z
NXP Employee
NXP Employee

QorIQ P1021/2010/2020 does not require for the SPI mode at boot time. The P2020 eSDHC does not support the SPI mode at all. The internal ROM SD/MMC driver supports 1-bit operation only (even if the SD/MMC card supports 4 or
8-bit parallel access). Of course ROM bootloader can load only small pard of the boot image, i.e. it can load code which reconfigures the eSDHC controller and load the rest.

0 Kudos