boot mode (LS1021A-IOT )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot mode (LS1021A-IOT )

Jump to solution
2,538 Views
myungjinhwang
Contributor III

I have some problems with LS1021A-IOT(SCH-28203 REV B3/700-28203 REV X2)

there are 2 boot mode in LS1021AIOT.

     - QSPI

     - SDHC(default)

I'd like to flash images and boot from QSPI.

I just changed SW2.1 (1 ->0).

But it's not work at all.

Question.

#1 : QSPI boot is supported ?

     - 6. Functional status and known limitations  (QSPI Boot No) in LS1021A-IOTGS.pdf

#2 : Should I control some others for QSPI boot?

#3 : i can see about TWR-LS1021A in QorIQ SDK 1.7 Documentation

      but no LS1021A-IOT. where may i see it ?

     - http://www.freescale.com/infocenter/index.jsp?topic=%2Fqfamily-sdk%2Findex.html

1 Solution
1,954 Views
artsiomstaliaro
Contributor IV

Check please uboot log:

U-Boot 2014.07+ls1+g659b6a2 (Jun 09 2015 - 05:54:30)

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

Where - 0x87081110 - Rev 1.0

View solution in original post

6 Replies
1,954 Views
artsiomstaliaro
Contributor IV

Please check this thread LS1021a-twr Unable to boot from QSPI

1,954 Views
myungjinhwang
Contributor III

Thanks for your reply...

this develop board is LS1021A-IOT(SCH-28203 REV B3/700-28203 REV X2)

where can i check more device rev?

if it is REV 1.0 or 2.0

Thank you.

0 Kudos
1,955 Views
artsiomstaliaro
Contributor IV

Check please uboot log:

U-Boot 2014.07+ls1+g659b6a2 (Jun 09 2015 - 05:54:30)

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

Where - 0x87081110 - Rev 1.0

1,954 Views
myungjinhwang
Contributor III

Thanks a lot^^

I should re check your reply thorougthly.

Have a good day~~~~~~~~

0 Kudos
1,954 Views
Pavel
NXP Employee
NXP Employee

See documentation for the LS1021A-IOT on the following page:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=LS1021A-IoT&fsrch=1&sr=2&pageNum=1
This page contains also SDK for LS1021A-IOT board.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,954 Views
myungjinhwang
Contributor III

Thanks for your reply ~~~

I already check all pdf files at the atteched  site.

But i can not find the solutions^^

0 Kudos