Which eMMC for ls102x can advice?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which eMMC for ls102x can advice?

1,611 Views
andrey_knnv
Contributor III

Hi,

We used MTFC8GLDDQ-4M IT ( LBGA, 100-ball, 14x18x1.4 ) eMMC in our ls1020 based design (as boot source also).

But MTFC8GLDDQ-4M IT is EOL now unfortunately.

It looks like MTFC8GACAEDQ-AAT is the single choice for replacement, but it has 5.0 MMC Interface.

Is MTFC8GACAEDQ-AAT compatible with ls102x or not?

Can you suggest any replacement for MTFC8GLDDQ-4M IT (8GB or more, LBGA, 100-ball, 14x18x1.4 )?

Tnx,

Andrey.

Tags (1)
0 Kudos
Reply
4 Replies

1,109 Views
twmemphis
Contributor III

Hello Andrey,

on eMMC components, most manufacturers moved from 100 ball BGA to 153 ball BGA type parts as these are much more common. You will find numerous suppliers having these.

If you can, please modify your design to use 153 ball eMMC in the future. This will relax your supply situation a lot.

However, eMMC mostly just support a temperature range from -25 to 85°C.

I work at the specialzed distributor Memphis Electronic. We distribute only memory-devices such as DRAM or Flash, but carry almost all manufacturers. For our industrial customers worldwide who very often need eMMC with -40 to 85°C we decided to build up a large inventory of Hynix brand eMMCs from 8GB up to 64GB. These all come in 153 ball BGA , but they support the full industrial temperature range of -40 to 85°C and they are immediately available from our stock!

Regards,

Thorsten

0 Kudos
Reply

1,109 Views
andrey_knnv
Contributor III

Hi Thorsten,

We can't move our desing to use 153 ball eMMC at the moment unfortunately.

May be in the future design.

Thanks for suggestion anyway.

Br,

Andrey.

0 Kudos
Reply

1,109 Views
Pavel
NXP Employee
NXP Employee

The MTFC8GLDDQ-4M can be used on the LS1021a board.

 

Look at the following documents:

https://www.datalight.com/solutions/technologies/emmc/emmc-feature-comparison-by-version

 

and

 

https://community.nxp.com/docs/DOC-332187

 

and

 

https://www.jetone.com.tw/uploadfiles/327/datasheet/KSI/ksi-emmc-upsi.pdf

 

The eMMC 5.1 devices are back compatible to the eMMC 4.2. The DS signal is not used for the eMMC 4.5 controller.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,109 Views
andrey_knnv
Contributor III

Hi Pavel,

Thank you for detailed answer.

Regards,

Andrey.

0 Kudos
Reply