What is the "Packet Analysis Tool" product of LS1020A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the "Packet Analysis Tool" product of LS1020A?

401 Views
yasushihasegawa
Contributor III

Dear Community Team,

 

I think that there was QorIQ Optimization Suite (QOS) as a Packet Analysis Tool.

http://cache.freescale.com/files/training/doc/ftf/2014/FTF-SDS-F0004.pdf 

 

[Question]
When using LS1020A, now, what should I purchase Packet Analysis Tool?

 

Best Regards,
Yasushi Hasegawa

0 Kudos
1 Reply

328 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The Packet Analysis tool supports QorIQ devices which implement DPAA only. The LS1020A does not implements DPAA. For most applications, the libraries and communications drivers contained in the QorIQ Linux SDK will be more than enough to get the job done with best-in-class packet processing metrics.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos