But i was trying to Open Vox PCie card on the p2020 board but it is not detecting the card. dahdi drivers are installed. but dahdi_hardware does not find that card.
When i run lspci -v the following output comes :
0000:00:00.0 PCI bridge: Freescale Semiconductor Inc P2020E (rev 21) (prog-if 00 [Normal decode])
Flags: bus master, fast devsel, latency 0
Memory at <ignored> (32-bit, non-prefetchable)
Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
I/O behind bridge: 00000000-00000fff
Memory behind bridge: a0000000-bfffffff
Capabilities: [44] Power Management version 2
Capabilities: [4c] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
lspci: Unable to load libkmod resources: error -12
0000:01:00.0 Mass storage controller: Silicon Image, Inc. SiI 3132 Serial ATA Raid II Controller (rev 01)
Subsystem: Silicon Image, Inc. SiI 3132 Serial ATA Raid II Controller
Flags: bus master, fast devsel, latency 0, IRQ 24
Memory at a0000000 (64-bit, non-prefetchable) [size=128]
Memory at a0004000 (64-bit, non-prefetchable) [size=16K]
I/O ports at 1000 [size=128]
[virtual] Expansion ROM at a0080000 [disabled] [size=512K]
Capabilities: [54] Power Management version 2
Capabilities: [5c] MSI: Enable- Count=1/1 Maskable- 64bit+
Capabilities: [70] Express Legacy Endpoint, MSI 00
Capabilities: [100] Advanced Error Reporting
Kernel driver in use: sata_sil24
0001:02:00.0 PCI bridge: Freescale Semiconductor Inc P2020E (rev 21) (prog-if 00 [Normal decode])
Flags: bus master, fast devsel, latency 0
Memory at <ignored> (32-bit, non-prefetchable)
Bus: primary=00, secondary=03, subordinate=03, sec-latency=0
I/O behind bridge: 00000000-00000fff
Memory behind bridge: 80000000-9fffffff
Capabilities: [44] Power Management version 2
Capabilities: [4c] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
A quick response will be highly appreciated.
Please provide additional information:
1) P2020 to the PCIe card connection schematics as PDF
2) values of the PORBMSR and PORDEVSR
3) U-Boot booting log
4) measured frequency of the reference clock provided to the PCIe card
Please consider that it could be more convenient to create a Technical Case:
Please find below the answer to queries :
1) P2020 to the PCIe card connection schematics as PDF
It is P2020rdb development board from freescale which supports single x1 PCIe slot. PCIe car is inserted in that slot.
) values of the PORBMSR and PORDEVSR
How to find these values ?
3) U-Boot booting log
How to get U-boot Log
4) measured frequency of the reference clock provided to the PCIe card
how to find these values ?
1), 4) - not actual for the P2020RDB.
2) The requested log is printed by U-Boot on the console during the board booting.
3) Execute U-Boot command 'md ffee0000' and provide the log.
5) What are settings of all on-board switches?
Hi ufedor ,
PFB the U-boot logging during bootup :
U-Boot 2013.01-00115-g831b30d (Jun 14 2013 - 21:48:56)
CPU0: P2020E, Version: 2.1, (0x80ea0021)
Core: E500, Version: 5.1, (0x80211051)
Clock Configuration:
CPU0:1200 MHz, CPU1:1200 MHz,
CCB:600 MHz,
DDR:400 MHz (800 MT/s data rate) (Asynchronous), LBC:37.500 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P2020RDB-PCA CPLD: V4.2 PCBA: V4.0
rom_loc: nor upper bank
SD/MMC : 4-bit Mode
eSPI : Enabled
I2C: ready
SPI: ready
DRAM: Detected UDIMM
1 GiB (DDR3, 64-bit, CL=6, ECC off)
Flash: 16 MiB
L2: 512 KB enabled
NAND: 128 MiB
MMC: FSL_SDHC: 0
PCIe1: Root Complex of mini PCIe SLOT, no link, regs @ 0xffe0a000
PCIe1: Bus 00 - 00
PCIe2: Root Complex of PCIe SLOT, x1, regs @ 0xffe09000
02:00.0 - 10b5:8112 - Bridge device
03:00.0 - e159:0001 - Simple comm. controller
PCIe2: Bus 01 - 03
In: serial
Out: serial
Err: serial
Net: eTSEC2 is in sgmii mode.
uploading VSC7385 microcode from ef000000
PHY reset timed out
eTSEC1, eTSEC2, eTSEC3
2. Output of md ffee0000 as below :
=> md ffee0000
ffee0000: 4444180c 8f370000 00000000 0a713847 DD...7.......q8G
ffee0010: 05000000 8bff27f0 00000000 00000000 ......'.........
ffee0020: 00010000 00000000 00000000 00000000 ................
ffee0030: 00000000 00000000 00000000 00000000 ................
ffee0040: 00000000 00000000 00000000 00000000 ................
ffee0050: 00000000 00000000 00000000 00000000 ................
ffee0060: 60000000 00000000 00000000 00000000 `...............
ffee0070: 02080000 00000000 00000000 00000000 ................
ffee0080: 00000000 00000000 00000000 000000e0 ................
ffee0090: 00000000 00000000 00000000 0000c000 ................
ffee00a0: 80211051 80ea0021 00000010 00000000 .!.Q...!........
ffee00b0: 00000000 00000000 00000000 00000000 ................
ffee00c0: 00000331 00000000 00000000 00000000 ...1............
ffee00d0: ffff0000 00000000 00000000 00000000 ................
ffee00e0: 00000000 00000000 00000000 00000000 ................
ffee00f0: 00000000 00000000 00000000 00000000 ................
3. Settings of all On-board Switches
DIP Switch SW 2:
SW2[1]= OFF
SW2[2-8]= ON
DIP Switch SW 3:
SW3[1-2]= ON
SW3[3-4]= OFF
SW3[5]= ON
SW3[6]= OFF
SW3[7]= ON
SW3[8]= OFF
From the log:
PCIe2: Root Complex of PCIe SLOT, x1, regs @ 0xffe09000
02:00.0 - 10b5:8112 - Bridge device
03:00.0 - e159:0001 - Simple comm. controller
Which exactly device is not discovered - i.e. what are its Device ID and Vendor ID?
Finally device is detected , i just gave pci command on u-boot
the output is as follows :
root@p2020rdb:/lib/modules/3.12.19-rt30-QorIQ-SDK-V1.7+g6619b8b# lspci -v
0000:00:00.0 PCI bridge: Freescale Semiconductor Inc P2020E (rev 21) (prog-if 00 [Normal decode])
Flags: bus master, fast devsel, latency 0
Memory at <ignored> (32-bit, non-prefetchable)
Bus: primary=00, secondary=01, subordinate=02, sec-latency=0
I/O behind bridge: 00000000-00000fff
Memory behind bridge: a0000000-bfffffff
Capabilities: [44] Power Management version 2
Capabilities: [4c] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
lspci: Unable to load libkmod resources: error -12
0000:01:00.0 PCI bridge: PLX Technology, Inc. PEX8112 x1 Lane PCI Express-to-PCI Bridge (rev aa) (prog-if 00 [Normal decode])
Flags: bus master, fast devsel, latency 0
Bus: primary=01, secondary=02, subordinate=02, sec-latency=0
I/O behind bridge: 00001000-00001fff
Memory behind bridge: a0000000-a00fffff
Capabilities: [40] Power Management version 2
Capabilities: [50] MSI: Enable- Count=1/1 Maskable- 64bit+
Capabilities: [60] Express PCI-Express to PCI/PCI-X Bridge, MSI 00
Capabilities: [100] Power Budgeting <?>
0000:02:00.0 Communication controller: Tiger Jet Network Inc. Tiger3XX Modem/ISDN interface
Subsystem: OpenVox Communication Co. Ltd. OpenVox A400P 4-port analog card
Flags: bus master, medium devsel, latency 128, IRQ 24
I/O ports at 1000 [size=256]
Memory at a0000000 (32-bit, non-prefetchable) [size=4K]
Capabilities: [40] Power Management version 2
0001:03:00.0 PCI bridge: Freescale Semiconductor Inc P2020E (rev 21) (prog-if 00 [Normal decode])
Flags: bus master, fast devsel, latency 0
Memory at <ignored> (32-bit, non-prefetchable)
Bus: primary=00, secondary=04, subordinate=04, sec-latency=0
I/O behind bridge: 00000000-00000fff
Memory behind bridge: 80000000-9fffffff
Capabilities: [44] Power Management version 2
Capabilities: [4c] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
But when i am trying to use dahdi_genconf the following error comes :
root@p2020rdb:/lib/modules/3.12.19-rt30-QorIQ-SDK-V1.7+g6619b8b# dah di_genconf
Can't locate Getopt/Long.pm in @INC (@INC contains: /usr/sbin /usr/sbin/perl_modules /etc/perl /usr/lib/perl/site_perl/5.14.3/ /usr/lib/perl/site_perl/5.14.3 /usr/lib/perl/vendor_perl/5.14.3/ /usr/lib/perl/vendor_perl/5.14.3 /usr/lib/perl/5.14.3/ /usr/lib/perl/5.14.3 /usr/local/lib/site_perl /usr/lib/perl/5.14.3 .) at /usr/sbin/dahdi_genconf line 14.
BEGIN failed--compilation aborted at /usr/sbin/dahdi_genconf line 14.
my perl -V cmd also gives right output
root@p2020rdb:/lib/modules/3.12.19-rt30-QorIQ-SDK-V1.7+g6619b8b# perl -v
This is perl 5, version 14, subversion 3 (v5.14.3) built for powerpc-linux-gnuspe
Copyright 1987-2012, Larry Wall
Perl may be copied only under the terms of either the Artistic License or the
GNU General Public License, which may be found in the Perl 5 source kit.
Complete documentation for Perl, including FAQ lists, should be found on
this system using "man perl" or "perldoc perl". If you have access to the
Internet, point your browser at http://www.perl.org/, the Perl Home Page.
root@p2020rdb:/lib/modules/3.12.19-rt30-QorIQ-SDK-V1.7+g6619b8b# perl -v V
Warning: failed to load Config_git.pl, something strange about this perl...
Summary of my perl5 (revision 5 version 14 subversion 2) configuration:
undef undef
Platform:
osname=linux, osvers=2.6.37-rc5-yocto-standard+, archname=powerpc-linux-gnuspe
uname='linux qemux86 2.6.37-rc5-yocto-standard+ #1 preempt mon dec 20 14:21:27 pst 2010 i686 gnulinux '
config_args='-des -Doptimize=-O2 -Dmyhostname=localhost -Dperladmin=root@localhost -Dcc=gcc -Dcf_by=Open Embedded -Dinstallprefix=/usr -Dprefix=/usr -Dvendorprefix=/usr -Dsiteprefix=/usr -Dotherlibdirs=/usr/lib/perl/5.14.3 -Duseshrplib -Dusethreads -Duseithreads -Duselargefiles -Ud_dosuid -Dd_semctl_semun -Ui_db -Ui_ndbm -Ui_gdbm -Di_shadow -Di_syslog -Dman3ext=3pm -Duseperlio -Dinstallusrbinperl -Ubincompat5005 -Uversiononly -Dpager=/usr/bin/less -isr'
hint=recommended, useposix=true, d_sigaction=define
useithreads=define, usemultiplicity=define
useperlio=define, d_sfio=undef, uselargefiles=define, usesocks=undef
use64bitint=undef, use64bitall=undef, uselongdouble=undef
usemymalloc=n, bincompat5005=undef
Compiler:
cc='powerpc-fsl-linux-gnuspe-gcc -m32 -mcpu=8548 -mabi=spe -mspe -mfloat-gprs=double ', ccflags =' -O2 -pipe -g -feliminate-unused-debug-types -DDEBIAN -D_REENTRANT -D_GNU_SOURCE -fno-strict-aliasing -pipe -fstack-protector -D_LARGEFILE_SOURCE -D_FILE_OFFSET_BITS=64',
optimize='-O2',
cppflags='-fno-strict-aliasing'
ccversion='', gccversion='4.5.1', gccosandvers=''
intsize=4, longsize=4, ptrsize=4, doublesize=8, byteorder=4321
d_longlong=define, longlongsize=8, d_longdbl=define, longdblsize=12
ivtype='long', ivsize=4, nvtype='double', nvsize=8, Off_t='off_t', lseeksize=8
alignbytes=4, prototype=define
Linker and Libraries:
ld='powerpc-fsl-linux-gnuspe-gcc -m32 -mcpu=8548 -mabi=spe -mspe -mfloat-gprs=double ', ldflags ='-Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed -fstack-protector'
libpth=/lib /usr/lib
libs=-lnsl -lgdbm -ldb -ldl -lm -lcrypt -lutil -lpthread -lc
perllibs=-lnsl -ldl -lm -lcrypt -lutil -lpthread -lc
libc=/lib/libc-2.12.1.so, so=so, useshrplib=true, libperl=libperl.so
gnulibc_version='2.12.1'
Dynamic Linking:
dlsrc=dl_dlopen.xs, dlext=so, d_dlsymun=undef, ccdlflags='-Wl,-E -Wl,-rpath,/usr/lib/perl/5.14.3//CORE'
cccdlflags='-fPIC', lddlflags='-Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed -fstack-protector -shared'
Characteristics of this binary (from libperl):
Compile-time options: MULTIPLICITY PERL_DONT_CREATE_GVSV
PERL_IMPLICIT_CONTEXT PERL_MALLOC_WRAP
PERL_PRESERVE_IVUV USE_ITHREADS USE_LARGE_FILES
USE_PERLIO USE_PERL_ATOF USE_REENTRANT_API
Built under linux
Compiled at Apr 29 2016 21:26:10
@INC:
/etc/perl
/usr/lib/perl/site_perl/5.14.3/
/usr/lib/perl/site_perl/5.14.3
/usr/lib/perl/vendor_perl/5.14.3/
/usr/lib/perl/vendor_perl/5.14.3
/usr/lib/perl/5.14.3/
/usr/lib/perl/5.14.3
/usr/local/lib/site_perl
/usr/lib/perl/5.14.3
In the original description you wrote:
> i was trying to Open Vox PCie card on the p2020 board but it is not detecting the card.
The card is now detected, so I believe that the issue is resolved and this thread has to be closed.
Please create new question for the new issue if you consider that it is connected with NXP/Freescale hardware or Linux SDK.
Hi ufedor ,
The issue seems to be linux kernel is installed is coming out to be 3.8.13 whereas my dahdi has been compiled with 3.12. I have used SDK 1.7 for building the complete linux image with dahdi . BUT kernel is always coming 3.8 as per below log though i have recompiled the kernel using following steps but still there is no change.
## Booting kernel from Legacy Image at ef080000 ...
Image Name: Linux-3.8.13-rt9-QorIQ-SDK-V1.4
Created: 2013-06-17 8:01:35 UTC
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 3602933 Bytes = 3.4 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
Uncompressing Kernel Image ... OK
please help seems to be very close to cracking it .
thanks in advance .
Hello Mohit,
We have a QorIQ based solution for Asterisk which is supporting 8 E1/T1 interfaces. You could try to redo everything and I will be happy to assist or you can get a complete solution which will save your time and effort.
Hi,
I had a similar problem with an NVMe hard disk on an LS2085A - drivers installed into the kernel, but the device isn't detected. I'm drawing a few (potentially incorrect) parallels between the P2020 and the LS2085A here, but:
How many lanes does your OpenVox PCIe card require? Are your PCIe slots on the P2020 configured correctly for the number of lanes on your OpenVox card?
Have you checked your SerDes configuration? In the LS2085A, the SerDes configuration can be tailored to support different numbers of lanes in each PCIe slot and you have to generate an RCW (reset configuration word) which reflects the configuration you want. The RCW is part of a PBL.bin file which is then uploaded to the board.
Looking in the QCVS tool, I created a default P2020 configuration project with DDR, HWDeviceTree and BOOTROM components. In the BOOTROM configuration Properties tab, the Power-On Reset Configuration contains a SerDes Configuration drop-down where you can inspect the Ref Clock, PLL timout, I/O port selection. It looks like the I/O port selection defaults to 0b1111, corresponding to
PCIe1 - 2 lanes
PCIe2 - 1 lane
PCIe3 - 1 lane
Which slot is your OpenVox card in? Based on your lspci output I presume you have a hard disk in PCIe2. Is it possible that the OpenVox card requires more PCIe lanes than is provided by the slot it is plugged into?
Also, is the device recognised in u-boot? There should be some lines like
PCIe1: Root Complex no link, regs @ 0x3600000
PCIe2: Root Complex no link, regs @ 0x3700000
PCIe3: disabled
What do these lines look like for your board?