Traffic bifurcation using DPDMUX on DPAA2 is not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Traffic bifurcation using DPDMUX on DPAA2 is not working

467 Views
Jeffrey_Lai
Contributor II

Hi NXP,

I try to verify Traffic bifurcation using DPDMUX on DPAA2 function on LX2160 according to the description of LSDK20.04 user guide, section 9.2.11.1.   

I use dpmac.3 and dpmac.17 to do the verification but it is not working. I always see dpdmux.0.1 link is down.

The attachment is the procedure log. Please help check the procedure is correct?

Thank you,

Jeffrey 

 

0 Kudos
Reply
1 Reply

119 Views
clarke_liu_f
Contributor I

Have you solved this problem? I have the same problem with LSDK21.08.

0 Kudos
Reply