The portion of the Security Monitor which is only on while the SoC is powered is referred to as the High Power (HP) section; the battery-backed portion is referred to as the Low Power (LP) section, and the TA_BB_VDD pin is the power supply to the LP section.
TA_BB_VDD should be connected to a power management IC (PMIC) which supplies 0.9 V or 1.0 V (same as VDD) from system power while the system is on, and switches to the supply source to a battery when the system is powered off.
There are special power sequencing and clocking requirements when using the battery-backed Security Monitor features on Trust 2.1 devices. Specifically, before allowing VDD to ramp up to the 0.5 V level, ensure that:
• OVDD has ramped to the recommended operational voltage
• DIFF_SYSCLK/DIFF_SYSCLK_B is running. This clock pair should have a minimum frequency of 800 Hz and a maximum frequency no greater than the maximum supported system clock frequency for the device.
Use of the LP section is optional.
If a Zeroizable Master Key or monotonic counter aren’t required to meet system trust objectives, TA_BB_VDD should be connected to VDD.
In our design we use the LP section.
If the TA_BB_VDD is supplied with the battery when the SoC is OFF and then Soc is turned ON how the requirement of "OVDD has ramped to the recommended operational voltage" is met whereas TA_BB_VDD is already ON when SoC is OFF?
If I switched TA_BB_VDD on VDD when I power the SoC then TA_BB_VDD will switch off until OVDD has ramped and Zeroizable Master Key will be deleted, right?