T2080 with a cps1616 srio switch,can sra work for only a srio port??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 with a cps1616 srio switch,can sra work for only a srio port??

812 Views
liguofa
Contributor III

Ask, can I use the sra example to test nwrite send and receive with only one srio port? As shown. If we can please give simple help. Thank you。

pastedImage_1.png

As shown in the figure, this port of our srio connects to an idt switch and is configured with a route. For example, the port of my srio is 0x11, and the routing port configuration I connect to is route to 0x11.

did sra can finish the test?we see the src and have not very clear about the law config for demo of sra.Can you give some more information about sra?

Tags (3)
0 Kudos
Reply
1 Reply

710 Views
yipingwang
NXP TechSupport
NXP TechSupport

sra> sra -attr port1 win_attr 1 nwrite nread (set port1 outbound window attribute to nwrite, nread)
sra> sra -op port1 1 0 0 s 0x100000 (set local memory to predefined data)
sra> sra -op port1 1 0 0 p 0x100000 (to see the memory data)
sra> sra -op port1 1 0 0 r 0x100000 (port1 reads 1M byte data and save them in port1's read data space)
sra> sra -op port1 1 0 0 p 0x100000 (to see whether read data is correct)

0 Kudos
Reply