Hi,
in the T1024 datasheet rev.1 at Table 1 the GPIO3_24/EC2_RX_DV when configured as GPIO is adviced to be tied to GND with a pull down (see note 14):
14. This pin requires an external 1-kΩ pull-down resistor to prevent PHY from seeing a valid Transmit Enable before it is actively driven.
This requirement seems strange as it cannot be configured as Trasmit Enable.
Is it an error?
Thanks,
Giacomo Gasparini