Hello
I try running a srio interface on my p2020 custom board. I plug a FPGA board with srio firmware to SRIO1 and configure SRIO as a host.
In uboot_config
configs/p1_p2_rdb_pc.h
#define CONFIG_SRIO1 /* SRIO port 1 */°
#define CONFIG_SYS_SRIO1_MEM_VIRT 0xC0000000
#define CONFIG_SYS_SRIO1_MEM_BUS 0xC0000000
#define CONFIG_SYS_SRIO1_MEM_PHYS CONFIG_SYS_SRIO1_MEM_BUS
#define CONFIG_SYS_SRIO1_MEM_SIZE 0x10000000 /* 256M */
tlb.c
SET_TLB_ENTRY(1, CONFIG_SYS_SRIO1_MEM_VIRT, CONFIG_SYS_SRIO1_MEM_PHYS,
MAS3_SX | MAS3_SW | MAS3_SR,°
MAS2_I | MAS2_G,
0, 3, BOOKE_PAGESZ_256M, 1),
Try to read srio memory from u-boot
=> md.l 0xc0000000
c0000000:
p2020 is stucked.
I can watch a read request and read response on FPGA board.
Why I can't read a srio memory?
Hello Andrei Petrukhin,
Please define the following in include/configs/p1_p2_rdb_pc.h.
#define CONFIG_SYS_SRIO
You could refer to the configuration for MPC8569MDS.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello, I have #define CONFIG_SYS_SRIO and other setting in the include/configs/p1_p2_rdb_pc.h. Now, I connete two P2020 processor one to another, by SRIO interface, and it's work! The problem was in the FGPA decvice. Thank you for your reply.