SHORT CIRCUITING VDD AND VDDC WHEN NOT USING DEEP SLEEP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SHORT CIRCUITING VDD AND VDDC WHEN NOT USING DEEP SLEEP

590 Views
xarowubas
Contributor III

Hello,

I'm designing a custom board around T1040. Since I'm not implementing deep sleep functionality, can I short circuit VDD and VDDC together and source them from single regulator ? This way they will both ramp up together. Will this cause any problem ?

Tags (4)
0 Kudos
1 Reply

499 Views
andrei_skok
NXP Employee
NXP Employee

According to the T1040 Datasheet, chapter 3.2 Power sequencing:

When Deep Sleep is not used, it is recommended to source VDD and VDDC from same power supply.


Have a great day,
Andrei

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos