Run the following command: sudo usr/sbin/visudo
Add the following line:
root ALL = NOPASSWD: /usr/bin/apt-get
Press CTRL-X for file saving.
Run script ”sudo ./poky/scripts/host-prepare.sh” again.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thanks.
It worked now.
At the later part of sdk installation, i am running the following command
--- source fsl-setup-poky -m p2020rdb
its saying
- "fsl-setup-poky directory not found"
Please suggest to resolve this.
Rgds,
Ankit
Use the following command:
source ./poky/fsl-setup-poky -m p2020rdb
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
It looks like that terminal window is open as root. Open terminal as uses.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------