Regarding tamper detection in P2041.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding tamper detection in P2041.

956 Views
sanakr
Contributor I

Hello,

 

I am using a P2041 QorIQ RDB board, and testing secure boot and tamper functionality on it. I am intending to simulate the tamper detection on this RDB board using the Switch 3.6 present on it. I could see the tamper evidence on U-boot, by accessing the register FE314018, wherethe value changes to 00000008 when a tamper occurs. I am intending to access this register using a module inserted in to the kernel, and activate tamper enable/disable selection from the linux prompt. As a newbie to kernel programming, I have tried to access the register as such using offset as given in the reference manual. I am getting a segmentation fault. Are there any macros available that can be used for accesing the security monitor registers in P2041 board? If yes, where might I find the details of them?

 

Thank you,

 

0 Kudos
Reply
1 Reply

763 Views
scottwood
NXP Employee
NXP Employee

The "offset as given in the reference manual" is not the same as an effective address that you can dereference.  In a Linux driver you need to use ioremap() to map a physical address to an effective address -- or better, use of_iomap() to map a resource from the device tree.

0 Kudos
Reply