QorIQ SDK v.2.5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QorIQ SDK v.2.5

2,020 次查看
dlciii
Contributor I

Hi, 

We just purchased the LX2160ARDB development system. Upon booting up the device we noticed a reference to QorIQ SDK v2.5.

The only version I see on your website is #qoriq_sdk_v2.0 (with the add-on of addendum 1703). The qoriq_sdk_v2.0 does not include the LX2160ARDB.

Is QorIQ v2.5 available for download?

If not, when will it be available for download?

Thanks.

标记 (1)
0 项奖励
回复
5 回复数

1,264 次查看
dlciii
Contributor I

Is there a QorIQ Yocto SDK update to version 2.5, similar to the QorIQ SDK referred to in the pdf documentation, QorIQ-SDK-2.0-1703-IC-Rev0.pdf?

Or is layerscape the only software development kit for the LX2160ARDB?

0 项奖励
回复

1,264 次查看
ufedor
NXP Employee
NXP Employee

> Is there a QorIQ Yocto SDK update to version 2.5

No.

Full integration of LX2160A will be implemented in the LSDK v19.03 (planned release - end of March)

0 项奖励
回复

1,264 次查看
dlciii
Contributor I

NOTE: "QorIQ SDK (FSL Reference Distro) 2.5 lx2160ardb /dev/ttyAMA0" at the bottom of this boot up sequence.

U-Boot 2017.07+fsl+g216f8f7 (Oct 12 2018 - 07:52:00 +0000)

SoC: LX2160ACE Rev1.0 (0x87360010)
Clock Configuration:
CPU0(A72):2000 MHz CPU1(A72):2000 MHz CPU2(A72):2000 MHz
CPU3(A72):2000 MHz CPU4(A72):2000 MHz CPU5(A72):2000 MHz
CPU6(A72):2000 MHz CPU7(A72):2000 MHz CPU8(A72):2000 MHz
CPU9(A72):2000 MHz CPU10(A72):2000 MHz CPU11(A72):2000 MHz
CPU12(A72):2000 MHz CPU13(A72):2000 MHz CPU14(A72):2000 MHz
CPU15(A72):2000 MHz
Bus: 700 MHz DDR: 2900 MT/s
Reset Configuration Word (RCW):
00000000: 50777738 1c500050 00000000 00000000
00000010: 00000000 0c010000 00000000 00000000
00000020: 010001a0 00002580 00000000 00000096
00000030: 00000000 00000000 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 00027000 00000000
00000070: 08b30010 001d0020
Model: NXP Layerscape LX2160ARDB Board
Board: LX2160ACE Rev1.0-RDB, Board version: B, boot from FlexSPI DEV#0
FPGA: v5.0
SERDES1 Reference: Clock1 = 161.13MHz Clock2 = 161.13MHz
SERDES2 Reference: Clock1 = 100MHz Clock2 = 100MHz
SERDES3 Reference: Clock1 = 100MHz Clock2 = 100Hz
I2C: ready
DRAM: Initializing DDR....using SPD
Detected UDIMM 18ADF2G72AZ-3G2E1
Detected UDIMM 18ADF2G72AZ-3G2E1
DDR4(0) UDIMM with 2-rank 64-bit bus (x8)
DDR4(1) UDIMM with 2-rank 64-bit bus (x8)
31.9 GiB
DDR 31.9 GiB (DDR4, 64-bit, CL=22, ECC on)
DDR Controller Interleaving Mode: 256B
DDR Chip-Select Interleaving Mode: CS0+CS1
VID: Core voltage after adjustment is at 801 mV
PPA Firmware: Version lx2160a-early-access-bsp0.1-p2
Using SERDES1 Protocol: 19 (0x13)
Using SERDES2 Protocol: 5 (0x5)
Using SERDES3 Protocol: 2 (0x2)
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected mt35xu512g with page size 256 Bytes, erase size 128 KiB, total 64 MiB
*** Warning - bad CRC, using default environment

EEPROM: NXID v1
In: serial_pl01x
Out: serial_pl01x
Err: serial_pl01x
SATA link 0 timeout.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
Found 0 device(s).
SCSI: Net:
CS4223: Using software initialization...
DPMAC3@xgmii: system interface USXGMII
DPMAC3@xgmii: Aquantia AQR107 Firmware Version 3.5.a
DPMAC4@xgmii: system interface USXGMII
DPMAC4@xgmii: Aquantia AQR107 Firmware Version 3.5.a
FSL_MDIO1:0 is connected to DPMAC5@25g-aui. Reconnecting to DPMAC6@25g-aui
PCIe0: pcie@3400000 disabled
PCIe1: pcie@3500000 disabled
PCIe2: pcie@3600000 Root Complex: no link
PCIe3: pcie@3700000 disabled
PCIe4: pcie@3800000 Root Complex: no link
PCIe5: pcie@3900000 disabled
DPMAC2@xlaui4, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@25g-aui, DPMAC6@25g-aui, DPMAC17@rgmii-id, DPMAC18@rgmii-id
crc32+
fsl-mc: Booting Management Complex ... SUCCESS
fsl-mc: Management Complex booted (version: 10.11.2, boot status: 0x1)
Hit any key to stop autoboot: 0
fsl-mc: Deploying data path layout ... SUCCESS
SF: Detected mt35xu512g with page size 256 Bytes, erase size 128 KiB, total 64 MiB
device 0 offset 0x1000000, size 0x3000000
SF: 50331648 bytes @ 0x1000000 Read: OK
## Loading kernel from FIT Image at a0000000 ...
Using 'config@1' configuration
Trying 'kernel@1' kernel subimage
Description: ARM64 Linux kernel
Created: 2018-10-12 8:37:47 UTC
Type: Kernel Image
Compression: gzip compressed
Data Start: 0xa00000d4
Data Size: 9097188 Bytes = 8.7 MiB
Architecture: AArch64
OS: Linux
Load Address: 0x80080000
Entry Point: 0x80080000
Verifying Hash Integrity ... OK
## Loading ramdisk from FIT Image at a0000000 ...
Using 'config@1' configuration
Trying 'ramdisk@1' ramdisk subimage
Description: Ramdisk
Created: 2018-10-12 8:37:47 UTC
Type: RAMDisk Image
Compression: uncompressed
Data Start: 0xa08b2408
Data Size: 8000429 Bytes = 7.6 MiB
Architecture: AArch64
OS: Linux
Load Address: unavailable
Entry Point: unavailable
Verifying Hash Integrity ... OK
## Loading fdt from FIT Image at a0000000 ...
Using 'config@1' configuration
Trying 'fdt@1' fdt subimage
Description: Flattened Device Tree blob
Created: 2018-10-12 8:37:47 UTC
Type: Flat Device Tree
Compression: uncompressed
Data Start: 0xa08ad16c
Data Size: 21019 Bytes = 20.5 KiB
Architecture: AArch64
Verifying Hash Integrity ... OK
Loading fdt from 0xa08ad16c to 0x90000000
Booting using the fdt blob at 0x90000000
Uncompressing Kernel Image ... OK
reserving fdt memory region: addr=80000000 size=10000
Loading Device Tree to 000000009fff7000, end 000000009ffff21a ... OK
WARNING: fdt_fixup_stdout: could not read serial-1 alias: FDT_ERR_NOTFOUND
WARNING: No random number to set kaslr-seed

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.9.62+g266488b (oe-user@oe-host) (gcc version 7.3.0 (GCC) ) #1 SMP PREEMPT Fri Oct 12 07:50:55 UTC 2018
[ 0.000000] Boot CPU: AArch64 Processor [410fd083]
[ 0.000000] earlycon: pl11 at MMIO32 0x00000000021c0000 (options '')
[ 0.000000] bootconsole [pl11] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 16 MiB at 0x00000000fac00000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000027bfffffff]
[ 0.000000] NUMA: Adding memblock [0x80000000 - 0xfbdfffff] on node 0
[ 0.000000] NUMA: Adding memblock [0x2080000000 - 0x27bfffffff] on node 0
[ 0.000000] NUMA: Initmem setup node 0 [mem 0x80000000-0x27bfffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x27bffd6040-0x27bffd77ff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] Normal [mem 0x0000000100000000-0x00000027bfffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000fbdfffff]
[ 0.000000] node 0: [mem 0x0000002080000000-0x00000027bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000027bfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv0.2 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] percpu: Embedded 23 pages/cpu @ffff80273fe63000 s55000 r8192 d31016 u94208
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] Built 1 zonelists in Node order, mobility grouping on. Total pages: 7982592
[ 0.000000] Policy zone: Normal
[ 0.000000] Kernel command line: console=ttyAMA0,115200 root=/dev/ram0 earlycon=pl011,mmio32,0x21c0000 ramdisk_size=0x2000000 default_hugepagesz=1024m hugepagesz=1024m hugepages=2 pci=pcie_bus_perf
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] software IO TLB [mem 0xf6c00000-0xfac00000] (64MB) mapped at [ffff800076c00000-ffff80007abfffff]
[ 0.000000] Memory: 29720360K/32438272K available (12732K kernel code, 1066K rwdata, 4880K rodata, 1152K init, 1006K bss, 2701528K reserved, 16384K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)
[ 0.000000] .text : 0xffff000008080000 - 0xffff000008cf0000 ( 12736 KB)
[ 0.000000] .rodata : 0xffff000008cf0000 - 0xffff0000091c0000 ( 4928 KB)
[ 0.000000] .init : 0xffff0000091c0000 - 0xffff0000092e0000 ( 1152 KB)
[ 0.000000] .data : 0xffff0000092e0000 - 0xffff0000093eaa00 ( 1067 KB)
[ 0.000000] .bss : 0xffff0000093eaa00 - 0xffff0000094e6354 ( 1007 KB)
[ 0.000000] fixed : 0xffff7dfffe7fd000 - 0xffff7dfffec00000 ( 4108 KB)
[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)
[ 0.000000] 0xffff7e0000000000 - 0xffff7e009d000000 ( 2512 MB actual)
[ 0.000000] memory : 0xffff800000000000 - 0xffff802740000000 (160768 MB)
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 64.
[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=16.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=16
[ 0.000000] NR_IRQS:64 nr_irqs:64 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] ITS [mem 0x06020000-0x0603ffff]
[ 0.000000] ITS@0x0000000006020000: allocated 65536 Devices @27a0880000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GIC: using LPI property table @0x00000027a0820000
[ 0.000000] ITS: Allocated 1792 chunks for LPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000006200000
[ 0.000000] CPU0: using LPI pending table @0x00000027a0830000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] arm_arch_timer: Architected cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000001] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns
[ 0.008340] Console: colour dummy device 80x25
[ 0.012856] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)
[ 0.023322] pid_max: default: 32768 minimum: 301
[ 0.028063] Security Framework initialized
[ 0.035131] Dentry cache hash table entries: 4194304 (order: 13, 33554432 bytes)
[ 0.050388] Inode-cache hash table entries: 2097152 (order: 12, 16777216 bytes)
[ 0.060973] Mount-cache hash table entries: 65536 (order: 7, 524288 bytes)
[ 0.067969] Mountpoint-cache hash table entries: 65536 (order: 7, 524288 bytes)
[ 0.075956] ASID allocator initialised with 65536 entries
[ 0.113459] PCI/MSI: /interrupt-controller@6000000/gic-its@6020000 domain created
[ 0.121063] Platform MSI: /interrupt-controller@6000000/gic-its@6020000 domain created
[ 0.129240] EFI services will not be available.
[ 0.181942] Detected PIPT I-cache on CPU1
[ 0.181956] GICv3: CPU1: found redistributor 1 region 0:0x0000000006220000
[ 0.181979] CPU1: using LPI pending table @0x000000279d770000
[ 0.181998] CPU1: Booted secondary processor [410fd083]
[ 0.213958] Detected PIPT I-cache on CPU2
[ 0.213971] GICv3: CPU2: found redistributor 100 region 0:0x0000000006240000
[ 0.213994] CPU2: using LPI pending table @0x000000279d7b0000
[ 0.214013] CPU2: Booted secondary processor [410fd083]
[ 0.245978] Detected PIPT I-cache on CPU3
[ 0.245986] GICv3: CPU3: found redistributor 101 region 0:0x0000000006260000
[ 0.246007] CPU3: using LPI pending table @0x000000279d7f0000
[ 0.246023] CPU3: Booted secondary processor [410fd083]
[ 0.278003] Detected PIPT I-cache on CPU4
[ 0.278015] GICv3: CPU4: found redistributor 200 region 0:0x0000000006280000
[ 0.278037] CPU4: using LPI pending table @0x000000279d020000
[ 0.278055] CPU4: Booted secondary processor [410fd083]
[ 0.310025] Detected PIPT I-cache on CPU5
[ 0.310034] GICv3: CPU5: found redistributor 201 region 0:0x00000000062a0000
[ 0.310055] CPU5: using LPI pending table @0x000000279d060000
[ 0.310071] CPU5: Booted secondary processor [410fd083]
[ 0.342050] Detected PIPT I-cache on CPU6
[ 0.342063] GICv3: CPU6: found redistributor 300 region 0:0x00000000062c0000
[ 0.342085] CPU6: using LPI pending table @0x000000279d0a0000
[ 0.342102] CPU6: Booted secondary processor [410fd083]
[ 0.374073] Detected PIPT I-cache on CPU7
[ 0.374083] GICv3: CPU7: found redistributor 301 region 0:0x00000000062e0000
[ 0.374104] CPU7: using LPI pending table @0x000000279d0e0000
[ 0.374119] CPU7: Booted secondary processor [410fd083]
[ 0.406102] Detected PIPT I-cache on CPU8
[ 0.406116] GICv3: CPU8: found redistributor 400 region 0:0x0000000006300000
[ 0.406138] CPU8: using LPI pending table @0x000000279d120000
[ 0.406156] CPU8: Booted secondary processor [410fd083]
[ 0.438124] Detected PIPT I-cache on CPU9
[ 0.438135] GICv3: CPU9: found redistributor 401 region 0:0x0000000006320000
[ 0.438155] CPU9: using LPI pending table @0x000000279d150000
[ 0.438171] CPU9: Booted secondary processor [410fd083]
[ 0.470149] Detected PIPT I-cache on CPU10
[ 0.470165] GICv3: CPU10: found redistributor 500 region 0:0x0000000006340000
[ 0.470186] CPU10: using LPI pending table @0x000000279d190000
[ 0.470204] CPU10: Booted secondary processor [410fd083]
[ 0.502172] Detected PIPT I-cache on CPU11
[ 0.502183] GICv3: CPU11: found redistributor 501 region 0:0x0000000006360000
[ 0.502204] CPU11: using LPI pending table @0x000000279d1d0000
[ 0.502219] CPU11: Booted secondary processor [410fd083]
[ 0.534200] Detected PIPT I-cache on CPU12
[ 0.534216] GICv3: CPU12: found redistributor 600 region 0:0x0000000006380000
[ 0.534238] CPU12: using LPI pending table @0x000000279d210000
[ 0.534256] CPU12: Booted secondary processor [410fd083]
[ 0.566222] Detected PIPT I-cache on CPU13
[ 0.566234] GICv3: CPU13: found redistributor 601 region 0:0x00000000063a0000
[ 0.566255] CPU13: using LPI pending table @0x000000279d250000
[ 0.566271] CPU13: Booted secondary processor [410fd083]
[ 0.598246] Detected PIPT I-cache on CPU14
[ 0.598263] GICv3: CPU14: found redistributor 700 region 0:0x00000000063c0000
[ 0.598286] CPU14: using LPI pending table @0x000000279d280000
[ 0.598303] CPU14: Booted secondary processor [410fd083]
[ 0.630269] Detected PIPT I-cache on CPU15
[ 0.630282] GICv3: CPU15: found redistributor 701 region 0:0x00000000063e0000
[ 0.630302] CPU15: using LPI pending table @0x000000279d2c0000
[ 0.630318] CPU15: Booted secondary processor [410fd083]
[ 0.630354] Brought up 16 CPUs
[ 0.969056] SMP: Total of 16 processors activated.
[ 0.973895] CPU features: detected feature: GIC system register CPU interface
[ 0.981107] CPU features: detected feature: 32-bit EL0 Support
[ 0.987055] CPU: All CPU(s) started at EL2
[ 0.991666] devtmpfs: initialized
[ 0.996960] DMI not present or invalid.
[ 1.000938] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 1.010820] futex hash table entries: 4096 (order: 6, 262144 bytes)
[ 1.017387] xor: measuring software checksum speed
[ 1.062246] 8regs : 8526.000 MB/sec
[ 1.106485] 8regs_prefetch: 7424.000 MB/sec
[ 1.151077] 32regs : 9606.000 MB/sec
[ 1.195316] 32regs_prefetch: 7858.000 MB/sec
[ 1.199979] xor: using function: 32regs (9606.000 MB/sec)
[ 1.205436] pinctrl core: initialized pinctrl subsystem
[ 1.211167] NET: Registered protocol family 16
[ 1.234440] cpuidle: using governor menu
[ 1.238458] fsl-mc MSI: /interrupt-controller@6000000/gic-its@6020000 domain created
[ 1.247964] arm-smmu 5000000.iommu: probing hardware configuration...
[ 1.254476] arm-smmu 5000000.iommu: SMMUv2 with:
[ 1.259140] arm-smmu 5000000.iommu: stage 1 translation
[ 1.264507] arm-smmu 5000000.iommu: stage 2 translation
[ 1.269873] arm-smmu 5000000.iommu: nested translation
[ 1.275153] arm-smmu 5000000.iommu: coherent table walk
[ 1.280519] arm-smmu 5000000.iommu: (IDR0.CTTW overridden by dma-coherent property)
[ 1.288349] arm-smmu 5000000.iommu: stream matching with 128 register groups, mask 0x7fff
[ 1.296706] arm-smmu 5000000.iommu: 64 context banks (0 stage-2 only)
[ 1.303305] arm-smmu 5000000.iommu: Supported page sizes: 0x61311000
[ 1.309814] arm-smmu 5000000.iommu: Stage-1: 48-bit VA -> 48-bit IPA
[ 1.316324] arm-smmu 5000000.iommu: Stage-2: 48-bit IPA -> 48-bit PA
[ 1.323233] vdso: 2 pages (1 code @ ffff000008cf7000, 1 data @ ffff0000092e5000)
[ 1.330714] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 1.337939] DMA: preallocated 256 KiB pool for atomic allocations
[ 1.344231] Serial: AMBA PL011 UART driver
[ 1.349080] Machine: NXP Layerscape LX2160ARDB
[ 1.353569] SoC family: QorIQ LX2160A
[ 1.357261] SoC ID: svr:0x87360010, Revision: 1.0
[ 1.363452] 21c0000.serial: ttyAMA0 at MMIO 0x21c0000 (irq = 94, base_baud = 0) is a SBSA
[ 1.371750] console [ttyAMA0] enabled
[ 1.371750] console [ttyAMA0] enabled
[ 1.379095] bootconsole [pl11] disabled
[ 1.379095] bootconsole [pl11] disabled
[ 1.386959] 21d0000.serial: ttyAMA1 at MMIO 0x21d0000 (irq = 95, base_baud = 0) is a SBSA
[ 1.396445] fsl_mc_bus 80c000000.fsl-mc: MC firmware version: 10.11.2
[ 1.405467] iommu: Adding device dprc.1 to group 0
[ 1.410406] fsl_mc_dprc dprc.1: cannot create uapi misc device
[ 1.446279] HugeTLB registered 1 GB page size, pre-allocated 2 pages
[ 1.519855] raid6: int64x1 gen() 1238 MB/s
[ 1.591857] raid6: int64x1 xor() 1160 MB/s
[ 1.663876] raid6: int64x2 gen() 1707 MB/s
[ 1.735900] raid6: int64x2 xor() 1652 MB/s
[ 1.807944] raid6: int64x4 gen() 2585 MB/s
[ 1.879972] raid6: int64x4 xor() 1743 MB/s
[ 1.952011] raid6: int64x8 gen() 2250 MB/s
[ 2.024025] raid6: int64x8 xor() 1748 MB/s
[ 2.096059] raid6: neonx1 gen() 2554 MB/s
[ 2.168098] raid6: neonx1 xor() 1711 MB/s
[ 2.240118] raid6: neonx2 gen() 3419 MB/s
[ 2.312149] raid6: neonx2 xor() 2592 MB/s
[ 2.384188] raid6: neonx4 gen() 4392 MB/s
[ 2.456215] raid6: neonx4 xor() 3311 MB/s
[ 2.528250] raid6: neonx8 gen() 4241 MB/s
[ 2.600284] raid6: neonx8 xor() 3303 MB/s
[ 2.604543] raid6: using algorithm neonx4 gen() 4392 MB/s
[ 2.609929] raid6: .... xor() 3311 MB/s, rmw enabled
[ 2.614882] raid6: using intx1 recovery algorithm
[ 2.619695] ACPI: Interpreter disabled.
[ 2.623652] RCPM: layerscape_rcpm_init: Can't find the RCPM node.
[ 2.629910] vgaarb: loaded
[ 2.632704] SCSI subsystem initialized
[ 2.636622] usbcore: registered new interface driver usbfs
[ 2.642120] usbcore: registered new interface driver hub
[ 2.647468] usbcore: registered new device driver usb
[ 2.652666] imx-i2c 2000000.i2c: can't get pinctrl, bus recovery not supported
[ 2.659967] i2c i2c-0: IMX I2C adapter registered
[ 2.664665] i2c i2c-0: can't use DMA, using PIO instead.
[ 2.670015] imx-i2c 2040000.i2c: can't get pinctrl, bus recovery not supported
[ 2.677299] i2c i2c-1: IMX I2C adapter registered
[ 2.681994] i2c i2c-1: can't use DMA, using PIO instead.
[ 2.687413] pps_core: LinuxPPS API ver. 1 registered
[ 2.692374] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 2.701503] PTP clock support registered
[ 2.705424] EDAC MC: Ver: 3.0.0
[ 2.708672] dmi: Firmware registration failed.
[ 2.713164] No BMan portals available!
[ 2.717044] QMan: Allocated lookup table at ffff00000ca01000, entry count 65537
[ 2.724400] No QMan portals available!
[ 2.728213] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 2.734303] Advanced Linux Sound Architecture Driver Initialized.
[ 2.740729] clocksource: Switched to clocksource arch_sys_counter
[ 2.746894] VFS: Disk quotas dquot_6.6.0
[ 2.750842] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 2.757805] pnp: PnP ACPI: disabled
[ 2.764222] NET: Registered protocol family 2
[ 2.768983] TCP established hash table entries: 262144 (order: 9, 2097152 bytes)
[ 2.776907] TCP bind hash table entries: 65536 (order: 8, 1048576 bytes)
[ 2.784021] TCP: Hash tables configured (established 262144 bind 65536)
[ 2.790700] UDP hash table entries: 16384 (order: 7, 524288 bytes)
[ 2.796995] UDP-Lite hash table entries: 16384 (order: 7, 524288 bytes)
[ 2.803785] NET: Registered protocol family 1
[ 2.808316] RPC: Registered named UNIX socket transport module.
[ 2.814229] RPC: Registered udp transport module.
[ 2.818925] RPC: Registered tcp transport module.
[ 2.823618] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 2.830128] Trying to unpack rootfs image as initramfs...
[ 2.835650] rootfs image is not initramfs (no cpio magic); looks like an initrd
[ 2.848948] Freeing initrd memory: 7808K
[ 2.853157] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 2.861000] kvm [1]: 8-bit VMID
[ 2.864129] kvm [1]: IDMAP page: 80ce1000
[ 2.868131] kvm [1]: HYP VA range: 800000000000:ffffffffffff
[ 2.874307] kvm [1]: Hyp mode initialized successfully
[ 2.879466] kvm [1]: vgic-v2@c0e0000
[ 2.883055] kvm [1]: GIC system register CPU interface enabled
[ 2.889058] kvm [1]: vgic interrupt IRQ1
[ 2.892982] kvm [1]: virtual timer IRQ4
[ 2.898212] audit: initializing netlink subsys (disabled)
[ 2.903621] audit: type=2000 audit(2.732:1): initialized
[ 2.909170] workingset: timestamp_bits=44 max_order=23 bucket_order=0
[ 2.916084] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 2.922064] NFS: Registering the id_resolver key type
[ 2.927115] Key type id_resolver registered
[ 2.931288] Key type id_legacy registered
[ 2.935291] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 2.942046] fuse init (API version 7.26)
[ 2.946042] SGI XFS with ACLs, security attributes, realtime, no debug enabled
[ 2.953600] 9p: Installing v9fs 9p2000 file system support
[ 2.959141] ceph: loaded (mds proto 32)
[ 2.964020] async_tx: api initialized (async)
[ 2.968400] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 2.975833] io scheduler noop registered
[ 2.979786] io scheduler cfq registered (default)
[ 2.985002] libphy: mdio_driver_register: phy-bcm-ns2-pci
[ 2.991423] OF: PCI: host bridge /soc/pcie@3600000 ranges:
[ 2.996909] OF: PCI: IO 0x9000020000..0x900002ffff -> 0x00000000
[ 3.003169] OF: PCI: MEM 0x9040000000..0x907fffffff -> 0x40000000
[ 4.009536] lx-pcie 3600000.pcie: phy link never came up
[ 4.014948] lx-pcie 3600000.pcie: PCI host bridge to bus 0000:00
[ 4.020950] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 4.026427] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 4.032600] pci_bus 0000:00: root bus resource [mem 0x9040000000-0x907fffffff] (bus address [0x40000000-0x7fffffff])
[ 4.043446] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 4.048691] pci 0000:00:00.0: Max Payload Size set to 256/ 256 (was 128), Max Read Rq 256
[ 4.057214] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 4.064393] OF: PCI: host bridge /soc/pcie@3800000 ranges:
[ 4.069877] OF: PCI: IO 0xa000020000..0xa00002ffff -> 0x00000000
[ 4.076137] OF: PCI: MEM 0xa040000000..0xa07fffffff -> 0x40000000
[ 5.082527] lx-pcie 3800000.pcie: phy link never came up
[ 5.087895] lx-pcie 3800000.pcie: PCI host bridge to bus 0001:00
[ 5.093896] pci_bus 0001:00: root bus resource [bus 00-ff]
[ 5.099374] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
[ 5.108322] pci_bus 0001:00: root bus resource [mem 0xa040000000-0xa07fffffff] (bus address [0x40000000-0x7fffffff])
[ 5.119230] pci 0001:00:00.0: PCI bridge to [bus 01-ff]
[ 5.124483] pci 0001:00:00.0: Max Payload Size set to 256/ 256 (was 128), Max Read Rq 256
[ 5.133006] pcieport 0001:00:00.0: Signaling PME through PCIe PME interrupt
[ 5.141200] Freescale LS2 console driver
[ 5.145166] fsl-ls2-console: device fsl_mc_console registered
[ 5.150940] fsl-ls2-console: device fsl_aiop_console registered
[ 5.157073] xenfs: not registering filesystem on non-xen platform
[ 5.164631] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 5.171513] SuperH (H)SCI(F) driver initialized
[ 5.176150] msm_serial: driver initialized
[ 5.185598] brd: module loaded
[ 5.191279] loop: module loaded
[ 5.194637] hisi_sas: driver version v1.6
[ 5.199027] ahci-qoriq 3200000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 5.207980] ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 5.217929] scsi host0: ahci-qoriq
[ 5.221420] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 97
[ 5.229379] ahci-qoriq 3210000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 5.238329] ahci-qoriq 3210000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 5.248209] scsi host1: ahci-qoriq
[ 5.251684] ata2: SATA max UDMA/133 mmio [mem 0x03210000-0x0321ffff] port 0x100 irq 98
[ 5.259644] ahci-qoriq 3220000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 5.268594] ahci-qoriq 3220000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 5.278492] scsi host2: ahci-qoriq
[ 5.281966] ata3: SATA max UDMA/133 mmio [mem 0x03220000-0x0322ffff] port 0x100 irq 99
[ 5.289921] ahci-qoriq 3230000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 5.298871] ahci-qoriq 3230000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 5.308753] scsi host3: ahci-qoriq
[ 5.312223] ata4: SATA max UDMA/133 mmio [mem 0x03230000-0x0323ffff] port 0x100 irq 100
[ 5.320712] nxp-fspi 20c0000.flexspi: mt35xu512aba (65536 Kbytes)
[ 5.327231] nxp-fspi 20c0000.flexspi: mt35xu512aba (65536 Kbytes)
[ 5.334356] libphy: Fixed MDIO Bus: probed
[ 5.338729] tun: Universal TUN/TAP device driver, 1.6
[ 5.343771] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[ 5.350010] CAN device driver interface
[ 5.353900] 2180000.can supply xceiver not found, using dummy regulator
[ 5.360738] flexcan 2180000.can: device registered (reg_base=ffff00000cf50000, irq=107)
[ 5.368744] 2190000.can supply xceiver not found, using dummy regulator
[ 5.375531] flexcan 2190000.can: device registered (reg_base=ffff00000cf70000, irq=108)
[ 5.383756] libphy: Freescale XGMAC MDIO Bus: probed
[ 5.392387] libphy: Freescale XGMAC MDIO Bus: probed
[ 5.398142] libphy: Freescale XGMAC MDIO Bus: probed
[ 5.403142] libphy: Freescale XGMAC MDIO Bus: probed
[ 5.408151] Freescale FM module, FMD API version 21.1.0
[ 5.413409] Freescale FM Ports module
[ 5.417062] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 5.422663] fsl_dpa: FSL DPAA Ethernet driver
[ 5.427039] fsl_advanced: FSL DPAA Advanced drivers:
[ 5.431993] fsl_proxy: FSL DPAA Proxy initialization driver
[ 5.437582] fsl_oh: FSL FMan Offline Parsing port driver
[ 5.443005] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 5.450042] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 5.455801] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 5.461624] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 5.467555] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.4.0-k
[ 5.474505] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 5.480088] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 5.487906] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 5.493834] sky2: driver version 1.30
[ 5.497843] VFIO - User Level meta-driver version: 0.3
[ 5.503952] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 5.510474] ehci-pci: EHCI PCI platform driver
[ 5.514941] ehci-platform: EHCI generic platform driver
[ 5.520214] ehci-exynos: EHCI EXYNOS driver
[ 5.524436] ehci-msm: Qualcomm On-Chip EHCI Host Controller
[ 5.530043] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 5.536221] ohci-pci: OHCI PCI platform driver
[ 5.540688] ohci-platform: OHCI generic platform driver
[ 5.542851] ata1: SATA link down (SStatus 0 SControl 300)
[ 5.551322] ohci-exynos: OHCI EXYNOS driver
[ 5.555612] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 5.561095] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 5.568901] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x02010010
[ 5.577609] xhci-hcd xhci-hcd.0.auto: irq 101, io mem 0x03100000
[ 5.578870] ata2: SATA link down (SStatus 0 SControl 300)
[ 5.589234] hub 1-0:1.0: USB hub found
[ 5.592985] hub 1-0:1.0: 1 port detected
[ 5.597006] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 5.602485] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 5.602850] ata3: SATA link down (SStatus 0 SControl 300)
[ 5.615536] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 5.623810] hub 2-0:1.0: USB hub found
[ 5.627559] hub 2-0:1.0: 1 port detected
[ 5.631597] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 5.634849] ata4: SATA link down (SStatus 0 SControl 300)
[ 5.642464] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
[ 5.650261] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x02010010
[ 5.658967] xhci-hcd xhci-hcd.1.auto: irq 102, io mem 0x03110000
[ 5.665164] hub 3-0:1.0: USB hub found
[ 5.668913] hub 3-0:1.0: 1 port detected
[ 5.672926] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 5.678406] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
[ 5.686071] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[ 5.694339] hub 4-0:1.0: USB hub found
[ 5.698088] hub 4-0:1.0: 1 port detected
[ 5.702223] usbcore: registered new interface driver usb-storage
[ 5.708584] mousedev: PS/2 mouse device common for all mice
[ 5.717310] rtc-pcf2127-i2c 1-0051: rtc core: registered rtc-pcf2127-i2c as rtc0
[ 5.724898] i2c /dev entries driver
[ 5.729476] i2c i2c-0: Added multiplexed i2c bus 2
[ 5.734376] i2c i2c-0: Added multiplexed i2c bus 3
[ 5.739292] i2c i2c-0: Added multiplexed i2c bus 4
[ 5.744236] i2c i2c-0: Added multiplexed i2c bus 5
[ 5.749101] i2c i2c-0: Added multiplexed i2c bus 6
[ 5.753968] i2c i2c-0: Added multiplexed i2c bus 7
[ 5.758830] i2c i2c-0: Added multiplexed i2c bus 8
[ 5.763693] i2c i2c-0: Added multiplexed i2c bus 9
[ 5.768478] pca954x 0-0077: registered 8 multiplexed busses for I2C mux pca9547
[ 5.778558] ina2xx 4-0040: power monitor ina220 (Rshunt = 500 uOhm)
[ 5.784846] 5-004c supply vcc not found, using dummy regulator
[ 5.794142] 5-004d supply vcc not found, using dummy regulator
[ 5.803020] sbsa-gwdt 23a0000.watchdog: Initialized with 30s timeout @ 25000000 Hz, action=0.
[ 5.811913] EDAC MC0: Giving out device to module fsl_ddr_edac controller fsl_mc_err: DEV fsl_mc_err (INTERRUPT)
[ 5.822109] fsl_ddr_edac acquired irq 85 for MC
[ 5.826630] fsl_ddr_edac MC err registered
[ 5.830910] EDAC MC1: Giving out device to module fsl_ddr_edac controller fsl_mc_err: DEV fsl_mc_err (INTERRUPT)
[ 5.841092] fsl_ddr_edac acquired irq 86 for MC
[ 5.845614] fsl_ddr_edac MC err registered
[ 5.850630] qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver
[ 5.857314] sdhci: Secure Digital Host Controller Interface driver
[ 5.863484] sdhci: Copyright(c) Pierre Ossman
[ 5.867922] Synopsys Designware Multimedia Card Interface Driver
[ 5.874097] sdhci-pltfm: SDHCI platform and OF driver helper
[ 5.916739] mmc0: SDHCI controller on 2140000.esdhc [2140000.esdhc] using ADMA 64-bit
[ 5.964743] mmc1: SDHCI controller on 2150000.esdhc [2150000.esdhc] using ADMA 64-bit
[ 5.972966] ledtrig-cpu: registered to indicate activity on CPUs
[ 5.979772] caam 8000000.crypto: device ID = 0x0a1a020000000000 (Era 10)
[ 5.986471] caam 8000000.crypto: job rings = 3, qi = 1
[ 6.000047] caam algorithms registered in /proc/crypto
[ 6.005191] caam 8000000.crypto: caam/qi frontend driver not suitable for DPAA 2.x, aborting...
[ 6.014526] caam_jr 8010000.jr: registering rng-caam
[ 6.019524] caam 8000000.crypto: caam pkc algorithms registered in /proc/crypto
[ 6.027053] usbcore: registered new interface driver usbhid
[ 6.032616] usbhid: USB HID core driver
[ 6.036520] DPAA2-ETH: debugfs created
[ 6.040422] No fsl,qman node
[ 6.043362] Freescale USDPAA process driver
[ 6.047535] fsl-usdpaa: no region found
[ 6.051369] Freescale USDPAA process IRQ driver
[ 6.053961] mmc1: new HS400 MMC card at address 0001
[ 6.054199] mmcblk1: mmc1:0001 R1J59E 116 GiB
[ 6.054314] mmcblk1boot0: mmc1:0001 R1J59E partition 1 8.00 MiB
[ 6.054428] mmcblk1boot1: mmc1:0001 R1J59E partition 2 8.00 MiB
[ 6.054544] mmcblk1rpmb: mmc1:0001 R1J59E partition 3 4.00 MiB
[ 6.083458] Netfilter messages via NETLINK v0.30.
[ 6.088328] nf_conntrack version 0.5.0 (65536 buckets, 262144 max)
[ 6.094568] nf_tables: (c) 2007-2009 Patrick McHardy <kaber@trash.net>
[ 6.101089] nf_tables_compat: (c) 2012 Pablo Neira Ayuso <pablo@netfilter.org>
[ 6.108473] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 6.113836] Initializing XFRM netlink socket
[ 6.118146] NET: Registered protocol family 10
[ 6.122983] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 6.129100] NET: Registered protocol family 17
[ 6.133543] NET: Registered protocol family 15
[ 6.137988] Bridge firewalling registered
[ 6.141990] Ebtables v2.0 registered
[ 6.145599] can: controller area network core (rev 20120528 abi 9)
[ 6.151789] NET: Registered protocol family 29
[ 6.156232] can: raw protocol (rev 20120528)
[ 6.160494] can: broadcast manager protocol (rev 20161123 t)
[ 6.166145] can: netlink gateway (rev 20130117) max_hops=1
[ 6.171657] 8021q: 802.1Q VLAN Support v1.8
[ 6.175852] 9pnet: Installing 9P2000 support
[ 6.180134] Key type dns_resolver registered
[ 6.184403] Key type ceph registered
[ 6.188062] libceph: loaded (mon/osd proto 15/24)
[ 6.193013] registered taskstats version 1
[ 6.197405] Btrfs loaded, crc32c=crc32c-generic
[ 6.243769] iommu: Adding device dpni.1 to group 0
[ 6.248577] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 6.254958] iommu: Adding device dpni.0 to group 0
[ 6.259758] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 6.266136] iommu: Adding device dpbp.1 to group 0
[ 6.270963] iommu: Adding device dpbp.0 to group 0
[ 6.275788] iommu: Adding device dpmac.18 to group 0
[ 6.280759] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 6.287137] iommu: Adding device dpmac.17 to group 0
[ 6.292108] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 6.298484] iommu: Adding device dpmac.6 to group 0
[ 6.303369] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 6.309746] iommu: Adding device dpmac.5 to group 0
[ 6.314631] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 6.321007] iommu: Adding device dpmac.4 to group 0
[ 6.325892] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 6.332269] iommu: Adding device dpmac.3 to group 0
[ 6.337154] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 6.343531] iommu: Adding device dpmac.2 to group 0
[ 6.348414] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 6.355268] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x130000 size 0x40
[ 6.363896] iommu: Adding device dpmcp.19 to group 0
[ 6.369372] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x120000 size 0x40
[ 6.377998] iommu: Adding device dpmcp.18 to group 0
[ 6.383475] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x110000 size 0x40
[ 6.392104] iommu: Adding device dpmcp.17 to group 0
[ 6.397578] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x100000 size 0x40
[ 6.406205] iommu: Adding device dpmcp.16 to group 0
[ 6.411681] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0xf0000 size 0x40
[ 6.420225] iommu: Adding device dpmcp.15 to group 0
[ 6.425701] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0xe0000 size 0x40
[ 6.434240] iommu: Adding device dpmcp.14 to group 0
[ 6.439716] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0xd0000 size 0x40
[ 6.448258] iommu: Adding device dpmcp.13 to group 0
[ 6.453733] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0xc0000 size 0x40
[ 6.462272] iommu: Adding device dpmcp.12 to group 0
[ 6.467749] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0xb0000 size 0x40
[ 6.476291] iommu: Adding device dpmcp.11 to group 0
[ 6.481766] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0xa0000 size 0x40
[ 6.490306] iommu: Adding device dpmcp.10 to group 0
[ 6.495782] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x90000 size 0x40
[ 6.504328] iommu: Adding device dpmcp.9 to group 0
[ 6.509716] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x80000 size 0x40
[ 6.518258] iommu: Adding device dpmcp.8 to group 0
[ 6.523648] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x70000 size 0x40
[ 6.532191] iommu: Adding device dpmcp.7 to group 0
[ 6.537580] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x60000 size 0x40
[ 6.546121] iommu: Adding device dpmcp.6 to group 0
[ 6.551511] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x50000 size 0x40
[ 6.560053] iommu: Adding device dpmcp.5 to group 0
[ 6.565442] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x40000 size 0x40
[ 6.573984] iommu: Adding device dpmcp.4 to group 0
[ 6.579374] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x30000 size 0x40
[ 6.587917] iommu: Adding device dpmcp.3 to group 0
[ 6.593306] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x20000 size 0x40
[ 6.601846] iommu: Adding device dpmcp.2 to group 0
[ 6.607237] fsl-mc: Got region 0 for obj type dpmcp base 0x80c000000 offset 0x10000 size 0x40
[ 6.615780] iommu: Adding device dpmcp.1 to group 0
[ 6.621175] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0x110000 size 0x1000
[ 6.630364] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x4110000 size 0x1000
[ 6.639641] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0x110000 size 0x10000
[ 6.648526] iommu: Adding device dpio.15 to group 0
[ 6.653917] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0x100000 size 0x1000
[ 6.663106] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x4100000 size 0x1000
[ 6.672383] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0x100000 size 0x10000
[ 6.681272] iommu: Adding device dpio.14 to group 0
[ 6.686663] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0xf0000 size 0x1000
[ 6.695766] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x40f0000 size 0x1000
[ 6.705047] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0xf0000 size 0x10000
[ 6.713848] iommu: Adding device dpio.13 to group 0
[ 6.719237] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0xe0000 size 0x1000
[ 6.728343] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x40e0000 size 0x1000
[ 6.737620] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0xe0000 size 0x10000
[ 6.746421] iommu: Adding device dpio.12 to group 0
[ 6.751811] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0xd0000 size 0x1000
[ 6.760920] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x40d0000 size 0x1000
[ 6.770198] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0xd0000 size 0x10000
[ 6.778997] iommu: Adding device dpio.11 to group 0
[ 6.784388] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0xc0000 size 0x1000
[ 6.793492] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x40c0000 size 0x1000
[ 6.802770] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0xc0000 size 0x10000
[ 6.811571] iommu: Adding device dpio.10 to group 0
[ 6.816967] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0xb0000 size 0x1000
[ 6.826072] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x40b0000 size 0x1000
[ 6.835348] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0xb0000 size 0x10000
[ 6.844148] iommu: Adding device dpio.9 to group 0
[ 6.849450] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0xa0000 size 0x1000
[ 6.858554] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x40a0000 size 0x1000
[ 6.867830] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0xa0000 size 0x10000
[ 6.876630] iommu: Adding device dpio.8 to group 0
[ 6.881933] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0x90000 size 0x1000
[ 6.891037] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x4090000 size 0x1000
[ 6.900313] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0x90000 size 0x10000
[ 6.909114] iommu: Adding device dpio.7 to group 0
[ 6.914418] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0x80000 size 0x1000
[ 6.923523] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x4080000 size 0x1000
[ 6.932804] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0x80000 size 0x10000
[ 6.941604] iommu: Adding device dpio.6 to group 0
[ 6.946909] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0x70000 size 0x1000
[ 6.956015] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x4070000 size 0x1000
[ 6.965293] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0x70000 size 0x10000
[ 6.974092] iommu: Adding device dpio.5 to group 0
[ 6.979398] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0x60000 size 0x1000
[ 6.988501] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x4060000 size 0x1000
[ 6.997779] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0x60000 size 0x10000
[ 7.006578] iommu: Adding device dpio.4 to group 0
[ 7.011883] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0x50000 size 0x1000
[ 7.020991] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x4050000 size 0x1000
[ 7.030266] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0x50000 size 0x10000
[ 7.039066] iommu: Adding device dpio.3 to group 0
[ 7.044370] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0x40000 size 0x1000
[ 7.053475] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x4040000 size 0x1000
[ 7.062751] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0x40000 size 0x10000
[ 7.071552] iommu: Adding device dpio.2 to group 0
[ 7.076862] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0x30000 size 0x1000
[ 7.085964] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x4030000 size 0x1000
[ 7.095241] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0x30000 size 0x10000
[ 7.104040] iommu: Adding device dpio.1 to group 0
[ 7.109344] fsl-mc: Got region 0 for obj type dpio base 0x818000000 offset 0x20000 size 0x1000
[ 7.118447] fsl-mc: Got region 1 for obj type dpio base 0x818000000 offset 0x4020000 size 0x1000
[ 7.127724] fsl-mc: Got region 2 for obj type dpio base 0x27f8000000 offset 0x20000 size 0x10000
[ 7.136523] iommu: Adding device dpio.0 to group 0
[ 7.141350] iommu: Adding device dpcon.31 to group 0
[ 7.146353] iommu: Adding device dpcon.30 to group 0
[ 7.151354] iommu: Adding device dpcon.29 to group 0
[ 7.156356] iommu: Adding device dpcon.28 to group 0
[ 7.161359] iommu: Adding device dpcon.27 to group 0
[ 7.166361] iommu: Adding device dpcon.26 to group 0
[ 7.171363] iommu: Adding device dpcon.25 to group 0
[ 7.176365] iommu: Adding device dpcon.24 to group 0
[ 7.181369] iommu: Adding device dpcon.23 to group 0
[ 7.186375] iommu: Adding device dpcon.22 to group 0
[ 7.191377] iommu: Adding device dpcon.21 to group 0
[ 7.196381] iommu: Adding device dpcon.20 to group 0
[ 7.201386] iommu: Adding device dpcon.19 to group 0
[ 7.206388] iommu: Adding device dpcon.18 to group 0
[ 7.211392] iommu: Adding device dpcon.17 to group 0
[ 7.216395] iommu: Adding device dpcon.16 to group 0
[ 7.221399] iommu: Adding device dpcon.15 to group 0
[ 7.226403] iommu: Adding device dpcon.14 to group 0
[ 7.231406] iommu: Adding device dpcon.13 to group 0
[ 7.236409] iommu: Adding device dpcon.12 to group 0
[ 7.241414] iommu: Adding device dpcon.11 to group 0
[ 7.246417] iommu: Adding device dpcon.10 to group 0
[ 7.251421] iommu: Adding device dpcon.9 to group 0
[ 7.256338] iommu: Adding device dpcon.8 to group 0
[ 7.261256] iommu: Adding device dpcon.7 to group 0
[ 7.266173] iommu: Adding device dpcon.6 to group 0
[ 7.271091] iommu: Adding device dpcon.5 to group 0
[ 7.276009] iommu: Adding device dpcon.4 to group 0
[ 7.280927] iommu: Adding device dpcon.3 to group 0
[ 7.285844] iommu: Adding device dpcon.2 to group 0
[ 7.290762] iommu: Adding device dpcon.1 to group 0
[ 7.295680] iommu: Adding device dpcon.0 to group 0
[ 7.306678] fsl_mc_dprc dprc.1: DPRC device bound to driver
[ 7.312264] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 7.318630] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 7.325004] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 7.331363] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 7.337720] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 7.344077] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 7.350433] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 7.356789] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 7.363147] fsl_mc_dprc dprc.1: No more resources of type dpmcp left
[ 7.371680] Mapped 0x27f8110000 to ffff00000d8b0000 size 65536
[ 7.378041] Using QMAN sharable memory cache
[ 7.382310] fsl_mc_dpio dpio.15: probed
[ 7.388170] Mapped 0x27f8100000 to ffff00000d8d0000 size 65536
[ 7.394526] Using QMAN sharable memory cache
[ 7.398793] fsl_mc_dpio dpio.14: probed
[ 7.404656] Mapped 0x27f80f0000 to ffff00000da10000 size 65536
[ 7.411010] Using QMAN sharable memory cache
[ 7.415275] fsl_mc_dpio dpio.13: probed
[ 7.421138] Mapped 0x27f80e0000 to ffff00000da30000 size 65536
[ 7.427491] Using QMAN sharable memory cache
[ 7.431756] fsl_mc_dpio dpio.12: probed
[ 7.437619] Mapped 0x27f80d0000 to ffff00000da50000 size 65536
[ 7.443972] Using QMAN sharable memory cache
[ 7.448237] fsl_mc_dpio dpio.11: probed
[ 7.454098] Mapped 0x27f80c0000 to ffff00000da70000 size 65536
[ 7.460451] Using QMAN sharable memory cache
[ 7.464716] fsl_mc_dpio dpio.10: probed
[ 7.470577] Mapped 0x27f80b0000 to ffff00000da90000 size 65536
[ 7.476933] Using QMAN sharable memory cache
[ 7.481198] fsl_mc_dpio dpio.9: probed
[ 7.486971] Mapped 0x27f80a0000 to ffff00000dab0000 size 65536
[ 7.493323] Using QMAN sharable memory cache
[ 7.497589] fsl_mc_dpio dpio.8: probed
[ 7.503362] Mapped 0x27f8090000 to ffff00000dad0000 size 65536
[ 7.509714] Using QMAN sharable memory cache
[ 7.513979] fsl_mc_dpio dpio.7: probed
[ 7.519754] Mapped 0x27f8080000 to ffff00000dc10000 size 65536
[ 7.526107] Using QMAN sharable memory cache
[ 7.530372] fsl_mc_dpio dpio.6: probed
[ 7.536146] Mapped 0x27f8070000 to ffff00000dc30000 size 65536
[ 7.542498] Using QMAN sharable memory cache
[ 7.546763] fsl_mc_dpio dpio.5: probed
[ 7.552537] Mapped 0x27f8060000 to ffff00000dc50000 size 65536
[ 7.558889] Using QMAN sharable memory cache
[ 7.563154] fsl_mc_dpio dpio.4: probed
[ 7.568929] Mapped 0x27f8050000 to ffff00000dc70000 size 65536
[ 7.575282] Using QMAN sharable memory cache
[ 7.579548] fsl_mc_dpio dpio.3: probed
[ 7.585323] Mapped 0x27f8040000 to ffff00000dc90000 size 65536
[ 7.591676] Using QMAN sharable memory cache
[ 7.595942] fsl_mc_dpio dpio.2: probed
[ 7.601716] Mapped 0x27f8030000 to ffff00000dcb0000 size 65536
[ 7.608068] Using QMAN sharable memory cache
[ 7.612333] fsl_mc_dpio dpio.1: probed
[ 7.618109] Mapped 0x27f8020000 to ffff00000dcd0000 size 65536
[ 7.624461] Using QMAN sharable memory cache
[ 7.628730] fsl_mc_dpio dpio.0: probed
[ 7.777621] fsl_dpaa2_eth dpni.1: Probed interface ni1
[ 7.927065] fsl_dpaa2_eth dpni.0: Probed interface ni0
[ 8.004837] Atheros 8035 ethernet 8b96000:02: at803x_config_init: LX2160ARDB packet loss workaround: disabling Smart EEE
[ 8.016518] dpaa2_mac dpmac.18: Connected to rgmii-id PHY.
[ 8.096836] Atheros 8035 ethernet 8b96000:01: at803x_config_init: LX2160ARDB packet loss workaround: disabling Smart EEE
[ 8.108514] dpaa2_mac dpmac.17: Connected to rgmii-id PHY.
[ 8.117983] dpaa2_mac dpmac.6: Registered fixed PHY.
[ 8.126611] dpaa2_mac dpmac.5: Registered fixed PHY.
[ 8.135152] dpaa2_mac dpmac.4: Connected to xgmii PHY.
[ 8.144458] dpaa2_mac dpmac.3: Connected to xgmii PHY.
[ 8.153842] dpaa2_mac dpmac.2: Registered fixed PHY.
[ 8.161773] rtc-pcf2127-i2c 1-0051: setting system clock to 2019-03-07 12:47:53 UTC (1551962873)
[ 8.170611] ALSA device list:
[ 8.173574] No soundcards found.
[ 8.177059] RAMDISK: gzip image found at block 0
[ 8.390472] EXT4-fs (ram0): couldn't mount as ext3 due to feature incompatibilities
[ 8.398454] EXT4-fs (ram0): mounted filesystem without journal. Opts: (null)
[ 8.405508] VFS: Mounted root (ext4 filesystem) readonly on device 1:0.
[ 8.412224] devtmpfs: mounted
[ 8.415504] Freeing unused kernel memory: 1152K
INIT: version 2.88 booting
Starting udev
[ 8.504225] udevd[1755]: starting version 3.2.5
[ 8.508913] random: udevd: uninitialized urandom read (16 bytes read)
[ 8.515387] random: udevd: uninitialized urandom read (16 bytes read)
[ 8.521871] random: udevd: uninitialized urandom read (16 bytes read)
[ 8.528326] random: udevd: uninitialized urandom read (16 bytes read)
[ 8.534784] random: udevd: uninitialized urandom read (16 bytes read)
[ 8.543919] udevd[1756]: starting eudev-3.2.5
[ 8.561060] random: udevd: uninitialized urandom read (16 bytes read)
[ 8.567519] random: udevd: uninitialized urandom read (16 bytes read)
[ 8.573974] random: udevd: uninitialized urandom read (16 bytes read)
[ 8.587960] random: udevd: uninitialized urandom read (16 bytes read)
[ 8.614122] random: udevd: uninitialized urandom read (16 bytes read)
[ 8.679932] EXT4-fs (ram0): re-mounted. Opts: (null)
Configuring packages on first boot....
(This may take several minutes. Please do not power off the machine.)
Running postinst /etc/rpm-postinsts/100-sysvinit-inittab...
INIT: Entering runlevel: 5un-postinsts exists during rc.d purg
Configuring network interfaces... done.
Starting OpenBSD Secure Shell server: sshd
generating ssh RSA key...
sync: ignoring all arguments
sync: ignoring all arguments
generating ssh ECDSA key...
sync: ignoring all arguments
sync: ignoring all arguments
generating ssh DSA key...
sync: ignoring all arguments
sync: ignoring all arguments
generating ssh ED25519 key...
sync: ignoring all arguments
sync: ignoring all arguments
done.
Starting syslogd/klogd: done

QorIQ SDK (FSL Reference Distro) 2.5 lx2160ardb /dev/ttyAMA0

lx2160ardb login: [ 71.588741] random: fast init done
[ 281.508750] random: crng init done

QorIQ SDK (FSL Reference Distro) 2.5 lx2160ardb /dev/ttyAMA0

lx2160ardb login: root
root@lx2160ardb:~# uname -a
Linux lx2160ardb 4.9.62+g266488b #1 SMP PREEMPT Fri Oct 12 07:50:55 UTC 2018 aarch64 GNU/Linux

0 项奖励
回复

1,264 次查看
ufedor
NXP Employee
NXP Employee

Provided log corresponds to the Layerscape LX2160A BSP v0.4

0 项奖励
回复

1,264 次查看
ufedor
NXP Employee
NXP Employee

> we noticed a reference to QorIQ SDK v2.5
What exactly doe you mean? Please provide corresponding log.
 

0 项奖励
回复