QorIQ LS1021A-IoT Security Engine Accelator Performance(with cryptodev)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QorIQ LS1021A-IoT Security Engine Accelator Performance(with cryptodev)

284件の閲覧回数
tecuelee
Contributor I

Hi,

I have one question about tilte.

How are these differences will appear?

# Openssl speed -evp aes-128-cbc -engine cryptodev -elapsed

type                16 bytes      64 bytes      256 bytes      1024 bytes      8192 bytes

aes-128-cbc   638.68k      2545.22k      8656.90k      32169.64k      137598.29k

# Openssl speed -evp aes-128-cbc -engine cryptodev

type                16 bytes           64 bytes           256 bytes      1024 bytes      8192 bytes

aes-128-cbc   10702.40k      44667.48k      184544.91k      683951.54k      5156556.80k

I want to use the hardware engine tries to configure the security network 1Gbps.

but I can not get satisfactory results.

Friendly seek your advice.

0 件の賞賛
0 返答(返信)