Pull up for POR configuration pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pull up for POR configuration pins

533 Views
rachanatm
Contributor II

I am using P1022 processor in my design. In checklist, it is mentioned that all POR configuration pins has internal pull up, which is enabled only during reset. In datasheet it is recomended to have pull/up or pull/dawn for some configuration pins. Is it really required to have pull up if default state is acceptable?

0 Kudos
1 Reply

428 Views
LPP
NXP Employee
NXP Employee

The checklist Section 3.1 is not consitent about internal pullups.

Just in the next section Table 4, the document provides comments for some signals as "There is no default value for this... must be pulled to desired value".

The configuration signals without default values do not provide internal pullups and should be pulled up/down externally. These recommendations conform to datasheet ones.

The configuration signals with default values do provide internal pullup during POR.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos