Is SRIO supported on t4240rdb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is SRIO supported on t4240rdb

830 Views
huiminshe
Contributor I

Hi,

I am trying to bring up SRIO on t4240rdb. However, the u-boot shows:

SRIO1: disabled

SRIO2: disabled

Does anyone know if t4240rdb supports SRIO?

If yes, how to enable it?

Thanks a lot.

/Huimin

0 Kudos
Reply
2 Replies

698 Views
LPP
NXP Employee
NXP Employee

T4240RDBUG Chapter 4

"

T4240RDB SerDes interface supports PCI Express, SATA II, and XFI data transfers.

T4240RDB supports 32 configurable SerDes:

• SerDes 1 lane E is configured as SGMII.

• SerDes 2 lane A to lane D is configured to support both XFI and SGMII (for 10Gbps

and 1Gbps speed).

• SerDes 3 lane A to lane H is configured as x8 PCIE port.

• SerDes 4 lane A to lane D is configured as x4 PCIE port.

• SerDes 4 lane 6 is configured as a SATA interface.

"

SRIO is not supported.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

698 Views
huiminshe
Contributor I

Thanks, Pavel.

Is it possible to somehow re-configure the RCW to enable SRIO?

Best regards,

Huimin

0 Kudos
Reply