PCIe support in Uboot LX2160A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe support in Uboot LX2160A

2,148件の閲覧回数
deepanrajanbara
Contributor IV

Hi,

Please let us know, PCIe is driver is supported in uboot. Also how to test the PCIe device is initialized without any issue in uboot.

Does the existing u-boot binary supports PCIe. or is there any sample board configuration in which PCI is enabled and initialized.

Thank you,

Deepanraj.A

ラベル(1)
0 件の賞賛
8 返答(返信)

1,927件の閲覧回数
ufedor
NXP Employee
NXP Employee

PCIe driver is supported in U-Boot.

You wrote:

> how to test the PCIe device is initialized without any issue in uboot.

U-Boot log will contain a line corresponding to each enabled PCIe controller.

This line will indicate the link training status. Trained link corresponds to properly enumerated EP device.

> Does the existing u-boot binary supports PCIe.

Yes, the LX2160A firmware contains U-Boot supporting PCIe.

0 件の賞賛

1,927件の閲覧回数
deepanrajanbara
Contributor IV

PCIe Gen2 and PCIe Gen3 is supported in u-boot ?

0 件の賞賛

1,927件の閲覧回数
ufedor
NXP Employee
NXP Employee

Specific PCIe protocol support details are determined by the RCW being used - not U-Boot itself.

0 件の賞賛

1,927件の閲覧回数
deepanrajanbara
Contributor IV

Does PCIe support QDMA in linux?

0 件の賞賛

1,927件の閲覧回数
ufedor
NXP Employee
NXP Employee

A PCIe controller can be used as source and/or destination of the qDMA - refer to the QorIQ LX2160A Reference Manual, Chapter 24 qDMA.

0 件の賞賛

1,927件の閲覧回数
deepanrajanbara
Contributor IV

Hi

Please share me the link to QorIQ LX2160A Reference Manual.

0 件の賞賛

1,927件の閲覧回数
ufedor
NXP Employee
NXP Employee

The RM is confidential and can be provided if NDA between NXP and your company is present.

Convenient way is to create a Technical Case:

https://support.nxp.com/s/ 

0 件の賞賛

1,927件の閲覧回数
deepanrajanbara
Contributor IV

Please reply for my Question

0 件の賞賛