P3041DS-PC - Aurora support?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P3041DS-PC - Aurora support?

355 次查看
miguelgarciacle
Contributor I

For our project we are looking for a Freescale board with VxWorks 7 BSP and Aurora debugging interface.

The P3041DS-PC is the only board that I have found with VxWorks 7 BSP and where in the high-level description it is explicitly mentioned that it has an Aurora connector.

Is it then the standard 70-pin connector? Can I then assume that the Aurora interface is working in that board (software support in the SDK)?

Thanks a lot

Miguel

0 项奖励
1 回复

284 次查看
ufedor
NXP Employee
NXP Employee

> Is it then the standard 70-pin connector

Yes, the board is equipped with standard 70-pin Aurora connector and supports Aurora (up to x2 lanes).

> Can I then assume that the Aurora interface is working in that board

Yes.

> (software support in the SDK)?

CodeWarrior supports Aurora.

0 项奖励