Hi NXP:
Our new design should update P2020's memory from DDR2 to DDR3.
But there is no ddr reset pin of P2020 mmu.
So, how can I deal with the ddr reset logic without CPLD?
Can connect the pin to Power on reset directly?
Billy Huan
B.R.
I got it.
Thanks a lot.
As DDR3 reset it is possible to use a copy of the reset signal going to the P2020's HRESET input.
never-displayed