P2020 external IRQ0 can't be triggered

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2020 external IRQ0 can't be triggered

756件の閲覧回数
yunyuaner
Contributor I

Hi,

I've set external IRQ0 to falling edge trigger and pulled this pin low, but it seem this interrupt doesn't be triggered, the corresponding interrupt service routine doesn't be called. The EIVPR0 and EIDR0 register values are:
PIC_EIVPR0 - 0x000c0001, PIC_EIDR0 - 0x00000001
Are there any other settings should be taken if I want to trigger external IRQ? (I've checked that EXT_IRQ0 isn't multiplexed with the other Pins)

Thanks!

Jia

タグ(3)
0 件の賞賛
返信
0 返答(返信)